<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: How does FlexIO clock(sck) will be generated in 8bit-baud mode?</title>
    <link>https://community.nxp.com/t5/S32K/How-does-FlexIO-clock-sck-will-be-generated-in-8bit-baud-mode/m-p/1050930#M6941</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The frequency of the transmission can be set by changing the value of the TIMCMP register&lt;/P&gt;&lt;P&gt;see the section "54.3.1.21 Timer Compare N Register (TIMCMP0 - TIMCMP3)"'&amp;nbsp; in the RM rev 12.1&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;In 8-bit baud counter mode, the lower 8-bits configure the baud rate divider equal to (CMP[7:0] + 1) * 2.&lt;BR /&gt;The upper 8-bits configure the number of bits in each word equal to (CMP[15:8] + 1) / 2.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can look at the doc Using FlexIO to emulate communications and timing peripherals&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12174.pdf" title="https://www.nxp.com/docs/en/application-note/AN12174.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12174.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;AN12174SW&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=AN12174SW&amp;amp;docLang=en" title="https://www.nxp.com/webapp/Download?colCode=AN12174SW&amp;amp;docLang=en"&gt;https://www.nxp.com/webapp/Download?colCode=AN12174SW&amp;amp;docLang=en&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Examples of the configuration can be found there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, a useful explanation of FlexIO is described on this link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105640"&gt;Understanding FlexIO&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Apr 2020 13:12:02 GMT</pubDate>
    <dc:creator>dianabatrlova</dc:creator>
    <dc:date>2020-04-21T13:12:02Z</dc:date>
    <item>
      <title>How does FlexIO clock(sck) will be generated in 8bit-baud mode?</title>
      <link>https://community.nxp.com/t5/S32K/How-does-FlexIO-clock-sck-will-be-generated-in-8bit-baud-mode/m-p/1050929#M6940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm configuring FlexIO for SPI, Even after going through the Reference manual (S32K148) I didn't understand how the serial clock will be generated from flexio using timer in 8bit-baud mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In manual it is like this -&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;When configured for 8-bit counter mode, whenever the lower 8-bit counter decrements to&lt;BR /&gt;zero the timer output will toggle, the lower 8-bit counter register will reload from the&lt;BR /&gt;compare register and the upper 8-bit counter will decrement&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;if it happens like above, clock output will not be proper right(There will not be 50% Duty cycle)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please someone make me understand how this clock will be generated in flexio SPI??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ravindra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Apr 2020 14:30:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-does-FlexIO-clock-sck-will-be-generated-in-8bit-baud-mode/m-p/1050929#M6940</guid>
      <dc:creator>ravihhk2</dc:creator>
      <dc:date>2020-04-18T14:30:35Z</dc:date>
    </item>
    <item>
      <title>Re: How does FlexIO clock(sck) will be generated in 8bit-baud mode?</title>
      <link>https://community.nxp.com/t5/S32K/How-does-FlexIO-clock-sck-will-be-generated-in-8bit-baud-mode/m-p/1050930#M6941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The frequency of the transmission can be set by changing the value of the TIMCMP register&lt;/P&gt;&lt;P&gt;see the section "54.3.1.21 Timer Compare N Register (TIMCMP0 - TIMCMP3)"'&amp;nbsp; in the RM rev 12.1&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;In 8-bit baud counter mode, the lower 8-bits configure the baud rate divider equal to (CMP[7:0] + 1) * 2.&lt;BR /&gt;The upper 8-bits configure the number of bits in each word equal to (CMP[15:8] + 1) / 2.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can look at the doc Using FlexIO to emulate communications and timing peripherals&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12174.pdf" title="https://www.nxp.com/docs/en/application-note/AN12174.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12174.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;AN12174SW&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=AN12174SW&amp;amp;docLang=en" title="https://www.nxp.com/webapp/Download?colCode=AN12174SW&amp;amp;docLang=en"&gt;https://www.nxp.com/webapp/Download?colCode=AN12174SW&amp;amp;docLang=en&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Examples of the configuration can be found there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, a useful explanation of FlexIO is described on this link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105640"&gt;Understanding FlexIO&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2020 13:12:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-does-FlexIO-clock-sck-will-be-generated-in-8bit-baud-mode/m-p/1050930#M6941</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2020-04-21T13:12:02Z</dc:date>
    </item>
    <item>
      <title>Re: How does FlexIO clock(sck) will be generated in 8bit-baud mode?</title>
      <link>https://community.nxp.com/t5/S32K/How-does-FlexIO-clock-sck-will-be-generated-in-8bit-baud-mode/m-p/1050931#M6942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/dianabatrlova"&gt;dianabatrlova&lt;/A&gt;‌, I understood the working of clock generation after going through&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-105640"&gt;https://community.nxp.com/docs/DOC-105640&lt;/A&gt;&amp;nbsp;link you shared.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ravindra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2020 09:05:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-does-FlexIO-clock-sck-will-be-generated-in-8bit-baud-mode/m-p/1050931#M6942</guid>
      <dc:creator>ravihhk2</dc:creator>
      <dc:date>2020-04-22T09:05:08Z</dc:date>
    </item>
    <item>
      <title>Re: How does FlexIO clock(sck) will be generated in 8bit-baud mode?</title>
      <link>https://community.nxp.com/t5/S32K/How-does-FlexIO-clock-sck-will-be-generated-in-8bit-baud-mode/m-p/1050932#M6943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Diana Batrlova&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is related to configuring DMA for multi byte transfer and keep chip select low for the entire bytes transfer complete.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With reference to example code for Design studio, we could succesfully send the data byte by byte.&lt;/P&gt;&lt;P&gt;However, as per requirement we want to do multiple byte transfer say128bytes and Chip select pin be low for the entire duration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly share your suggestions or pointers to look in related to this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jayakumar&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2020 15:14:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-does-FlexIO-clock-sck-will-be-generated-in-8bit-baud-mode/m-p/1050932#M6943</guid>
      <dc:creator>jaikumar81</dc:creator>
      <dc:date>2020-06-25T15:14:49Z</dc:date>
    </item>
    <item>
      <title>Re: How does FlexIO clock(sck) will be generated in 8bit-baud mode?</title>
      <link>https://community.nxp.com/t5/S32K/How-does-FlexIO-clock-sck-will-be-generated-in-8bit-baud-mode/m-p/1050933#M6944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to add the configuration:&lt;/P&gt;&lt;P&gt;baudRate: &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;400000U,&lt;BR /&gt; inputClock: &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;40000000U,&lt;BR /&gt; driverType: &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;FLEXIO_DRIVER_TYPE_DMA,&lt;BR /&gt; flexio_spi_transfer_bit_order_t: &amp;nbsp;&amp;nbsp;FLEXIO_SPI_TRANSFER_MSB_FIRST,&amp;nbsp;&lt;BR /&gt; flexio_spi_transfer_size_t: &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;FLEXIO_SPI_TRANSFER_2BYTE,&lt;/P&gt;&lt;P&gt;CLK_POL:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;CPOL_0;&lt;BR /&gt;CLK_PHA:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPHA_1 ;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SCK timer config :&amp;nbsp;&amp;nbsp;FLEXIO_TIMER_DISABLE_TIM_CMP(3)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MasterBugffer: Size 6 bytes&lt;/P&gt;&lt;P&gt;masterBuffer[0] = 0x06;&lt;BR /&gt; masterBuffer[1] = 0x14;&lt;BR /&gt; masterBuffer[2] = 0xF0;&lt;BR /&gt; masterBuffer[3] = 0x01;&lt;BR /&gt; masterBuffer[4] = 0x01;&lt;BR /&gt; masterBuffer[5] = 0xF4;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for(cnt=0; cnt&amp;lt; uBufLen; ++cnt)&lt;BR /&gt; {&lt;BR /&gt; FLEXIO_SPI_DRV_MasterTransfer(&amp;amp;SpiflexioStateMaster, &amp;amp;masterBuffer[0], NULL, 2);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following are the observations:&lt;/P&gt;&lt;P&gt;We have noticed that for 2 byte transmission(as per DMA configuration) is successful only for 2 bytes.&lt;/P&gt;&lt;P&gt;However, we could not notice the transmission for next consecutive&amp;nbsp; remaining bytes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, the way in single byte transmission we have noted DMA call back function being called is missing after updation of the DMA transfer size.&lt;/P&gt;&lt;P&gt;To be clear, after 2 byte transmission(as mentioned above) DMA call back function has missed thus I think further bytes are not processed for transmission.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;while, when we changed to&amp;nbsp;&lt;SPAN&gt;transfer_size_t:&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;FLEXIO_SPI_TRANSFER_4BYTE,, SPI_ENABLE is not going low.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We would like to know the missing configuration, such that DMA transfer is applicable for 128 bytes with Slave select low, through out the transmission, under single transfer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Kindly share your inputs.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Jayakumar Appari.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jun 2020 05:27:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-does-FlexIO-clock-sck-will-be-generated-in-8bit-baud-mode/m-p/1050933#M6944</guid>
      <dc:creator>jaikumar81</dc:creator>
      <dc:date>2020-06-26T05:27:14Z</dc:date>
    </item>
    <item>
      <title>Re: How does FlexIO clock(sck) will be generated in 8bit-baud mode?</title>
      <link>https://community.nxp.com/t5/S32K/How-does-FlexIO-clock-sck-will-be-generated-in-8bit-baud-mode/m-p/1050934#M6945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The issue is resolved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In one of the post, it has mentioned to use FlexioSPI (SPI_EN) as GPIO port to control the CS line.&lt;/P&gt;&lt;P&gt;Tried the same and behavior is as per expectation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Jun 2020 10:06:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-does-FlexIO-clock-sck-will-be-generated-in-8bit-baud-mode/m-p/1050934#M6945</guid>
      <dc:creator>jaikumar81</dc:creator>
      <dc:date>2020-06-28T10:06:40Z</dc:date>
    </item>
  </channel>
</rss>