<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Lpuart reception problem（S32K144 LPUART） in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Lpuart-reception-problem-S32K144-LPUART/m-p/1049299#M6904</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone!&lt;/P&gt;&lt;P&gt;When I use lpuart，there's a problem:&lt;/P&gt;&lt;P&gt;RX external pull down before initializing lpuart. In this way, the RDRF flag is set and the&amp;nbsp;DATA is 0, that is, a frame value of 0 can be received.&lt;/P&gt;&lt;P&gt;This is very strange, because I think the start bit received by UART&amp;nbsp;should have a falling edge.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 May 2020 01:52:26 GMT</pubDate>
    <dc:creator>ym1</dc:creator>
    <dc:date>2020-05-21T01:52:26Z</dc:date>
    <item>
      <title>Lpuart reception problem（S32K144 LPUART）</title>
      <link>https://community.nxp.com/t5/S32K/Lpuart-reception-problem-S32K144-LPUART/m-p/1049299#M6904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone!&lt;/P&gt;&lt;P&gt;When I use lpuart，there's a problem:&lt;/P&gt;&lt;P&gt;RX external pull down before initializing lpuart. In this way, the RDRF flag is set and the&amp;nbsp;DATA is 0, that is, a frame value of 0 can be received.&lt;/P&gt;&lt;P&gt;This is very strange, because I think the start bit received by UART&amp;nbsp;should have a falling edge.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 May 2020 01:52:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Lpuart-reception-problem-S32K144-LPUART/m-p/1049299#M6904</guid>
      <dc:creator>ym1</dc:creator>
      <dc:date>2020-05-21T01:52:26Z</dc:date>
    </item>
    <item>
      <title>Re: Lpuart reception problem（S32K144 LPUART）</title>
      <link>https://community.nxp.com/t5/S32K/Lpuart-reception-problem-S32K144-LPUART/m-p/1049300#M6905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what is the purpose of RX pull down and what is the connection you have?&lt;/P&gt;&lt;P&gt;UART transceiver should drive RX pin high for idle condition, so pull down has no effect and byte is normally received.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 May 2020 09:20:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Lpuart-reception-problem-S32K144-LPUART/m-p/1049300#M6905</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-05-21T09:20:26Z</dc:date>
    </item>
    <item>
      <title>Re: Lpuart reception problem（S32K144 LPUART）</title>
      <link>https://community.nxp.com/t5/S32K/Lpuart-reception-problem-S32K144-LPUART/m-p/1049301#M6906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;Before UART initialization, I multiplexed RX pin to GPIO, during which RX was pulled down.This is a special function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2020-05-22&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2020 00:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Lpuart-reception-problem-S32K144-LPUART/m-p/1049301#M6906</guid>
      <dc:creator>ym1</dc:creator>
      <dc:date>2020-05-22T00:37:13Z</dc:date>
    </item>
  </channel>
</rss>