<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Which register i need to set for CAN ID and Masking filter?</title>
    <link>https://community.nxp.com/t5/S32K/Which-register-i-need-to-set-for-CAN-ID-and-Masking-filter/m-p/1048692#M6888</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Team,&amp;nbsp;&lt;BR /&gt;For masking and filtering which register we need to set, so our Rx can allow only those message id to be received.&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/PetrS"&gt;PetrS&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;is it Rx Individual mask register for masking? and for id filtering from where id will be check if masking bit will be 1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Apr 2020 05:44:25 GMT</pubDate>
    <dc:creator>shivamshankarg</dc:creator>
    <dc:date>2020-04-02T05:44:25Z</dc:date>
    <item>
      <title>Which register i need to set for CAN ID and Masking filter?</title>
      <link>https://community.nxp.com/t5/S32K/Which-register-i-need-to-set-for-CAN-ID-and-Masking-filter/m-p/1048692#M6888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Team,&amp;nbsp;&lt;BR /&gt;For masking and filtering which register we need to set, so our Rx can allow only those message id to be received.&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/PetrS"&gt;PetrS&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;is it Rx Individual mask register for masking? and for id filtering from where id will be check if masking bit will be 1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2020 05:44:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Which-register-i-need-to-set-for-CAN-ID-and-Masking-filter/m-p/1048692#M6888</guid>
      <dc:creator>shivamshankarg</dc:creator>
      <dc:date>2020-04-02T05:44:25Z</dc:date>
    </item>
    <item>
      <title>Re: Which register i need to set for CAN ID and Masking filter?</title>
      <link>https://community.nxp.com/t5/S32K/Which-register-i-need-to-set-for-CAN-ID-and-Masking-filter/m-p/1048693#M6889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the Accepance mask registers are used to filter incoming ID. There is bit2bit correspondence between received ID, mask and programmed MB ID (or RXFIFO ID filter elements). The mask says if corresponding incoming ID bit is compared with programmed ID bit.&lt;/P&gt;&lt;P&gt;If mask bit is cleared the incoming ID bit is not compared, it is don’t care. If mask bit is set, then there must be exact match between incoming ID bit and programmed ID bit. To receive a message into a MB/RXFIFO all relevant bits with mask bit set must be equal to programmed one.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are following rules for message filtering for different FlexCAN module configuration (assume module with 32 MBs)&lt;/P&gt;&lt;P&gt;a) When MCR[FEN]=0, no RX FIFO&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MCR[IRMQ]=0: MB0-MB31 use RXGMASK except MB14 uses RX14MASK and MB15 used RX15MASK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MCR[&lt;SPAN&gt;IRMQ&lt;/SPAN&gt;]=1: MB0-MB31 use RXIMR0-RXIMR31&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;b) When MCR[FEN]=1, RX FIFO used&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MCR[&lt;SPAN&gt;IRMQ&lt;/SPAN&gt;]=0: all RX FIFO ID elements uses RXFGMASK, rest od MBs use RXGMASK except MB14 uses RX14MASK and MB15 used RX15MASK (only if MB14/15 are not occupied by RXFIFO ID table)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MCR[&lt;SPAN&gt;IRMQ&lt;/SPAN&gt;]=1: RX FIFO ID elements uses RXIMRx and RXFGMASK depending the CTRL2[RFFN] setting&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2020 11:25:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Which-register-i-need-to-set-for-CAN-ID-and-Masking-filter/m-p/1048693#M6889</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-04-02T11:25:18Z</dc:date>
    </item>
    <item>
      <title>Re: Which register i need to set for CAN ID and Masking filter?</title>
      <link>https://community.nxp.com/t5/S32K/Which-register-i-need-to-set-for-CAN-ID-and-Masking-filter/m-p/1170347#M8535</link>
      <description>&lt;P&gt;Hi PetrS ,&lt;/P&gt;&lt;P&gt;I need to filter CAN incoming messages from 0x00001561 to 0x00001567 .&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;MCR[FEN]=0, no RX FIFO used&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;MCR[IRMQ]=0,using only RXMGMASK&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;How to assign value of RXMGMASK for this CAN IDs ?&lt;/P&gt;&lt;P&gt;Should I use RXFGMASK also for filtering ?&lt;/P&gt;&lt;P&gt;Kindly explain the relationship between CAN ID, RXMGMASK and RXFGMASK .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Yogish&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2020 12:37:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Which-register-i-need-to-set-for-CAN-ID-and-Masking-filter/m-p/1170347#M8535</guid>
      <dc:creator>yogish_krishna</dc:creator>
      <dc:date>2020-10-20T12:37:05Z</dc:date>
    </item>
    <item>
      <title>Re: Which register i need to set for CAN ID and Masking filter?</title>
      <link>https://community.nxp.com/t5/S32K/Which-register-i-need-to-set-for-CAN-ID-and-Masking-filter/m-p/1584612#M20099</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/141698"&gt;@yogish_krishna&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The below API can filter 0x00001560 to 0x00001567. I hope this helps for you.&lt;/P&gt;&lt;P&gt;Mask value:&amp;nbsp;&amp;nbsp;0xFFFFFF8&lt;/P&gt;&lt;P&gt;FLEXCAN_DRV_SetRxIndividualMask(INST_FLEXCAN_CONFIG_1, MSG_TYPE_ID, MB_index , 0xFFFFFF8)&lt;/P&gt;&lt;P&gt;BR,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Krishan&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 12:44:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Which-register-i-need-to-set-for-CAN-ID-and-Masking-filter/m-p/1584612#M20099</guid>
      <dc:creator>krishan_saini</dc:creator>
      <dc:date>2023-01-18T12:44:15Z</dc:date>
    </item>
  </channel>
</rss>