<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K14x  Program running Ram or Flash？</title>
    <link>https://community.nxp.com/t5/S32K/S32K14x-Program-running-Ram-or-Flash/m-p/1047593#M6874</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The s32k142,debug arm program that I use jlinkv9.4 debug can run normally, but after burning program should not burn to flash, the program does not run after I restart, this also has boot foot to choose where program starts to run? I didn't find it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 May 2020 01:01:18 GMT</pubDate>
    <dc:creator>1603279584</dc:creator>
    <dc:date>2020-05-06T01:01:18Z</dc:date>
    <item>
      <title>S32K14x  Program running Ram or Flash？</title>
      <link>https://community.nxp.com/t5/S32K/S32K14x-Program-running-Ram-or-Flash/m-p/1047593#M6874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The s32k142,debug arm program that I use jlinkv9.4 debug can run normally, but after burning program should not burn to flash, the program does not run after I restart, this also has boot foot to choose where program starts to run? I didn't find it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2020 01:01:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K14x-Program-running-Ram-or-Flash/m-p/1047593#M6874</guid>
      <dc:creator>1603279584</dc:creator>
      <dc:date>2020-05-06T01:01:18Z</dc:date>
    </item>
    <item>
      <title>Re: S32K14x  Program running Ram or Flash？</title>
      <link>https://community.nxp.com/t5/S32K/S32K14x-Program-running-Ram-or-Flash/m-p/1047594#M6875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi&amp;nbsp;Yingkun,&lt;/DIV&gt;&lt;DIV&gt;Have you try to program the SDK examples?&lt;/DIV&gt;&lt;DIV&gt;I have try to test these examples. Did not see similar phenomenon on S32K142EVB.&lt;/DIV&gt;&lt;DIV&gt;If you are test your own project, would you please check if WDOG is enabled or feed WODG periodically.&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2020 01:40:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K14x-Program-running-Ram-or-Flash/m-p/1047594#M6875</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2020-05-08T01:40:04Z</dc:date>
    </item>
  </channel>
</rss>