<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: VLPS to RUN delay in S32K</title>
    <link>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045421#M6839</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeremy He,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, we are meassuring a delay of 500us from the PORT falling edge, which is the wakeup event, until the associated ISR is serviced.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be going on here? Maybe the system PLL is taking long to lock? Or what?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help or hint would be really appreciated. Because this makes no sense. Why the datasheet states max 17us but we can measure more than 500us.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Jul 2020 22:04:01 GMT</pubDate>
    <dc:creator>rmelizalde</dc:creator>
    <dc:date>2020-07-30T22:04:01Z</dc:date>
    <item>
      <title>VLPS to RUN delay</title>
      <link>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045419#M6837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are meassuring a delay of over 500us from a wakeup event (falling edge in PORT) until the micro processes the related interrupt (PORT).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This seems to be too much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We would like to get some support on this topic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Can we improve the wakeup reponse time?&lt;/P&gt;&lt;P&gt;- Is it specified somewhere the transition delay time from VLPS to RUN? In the past, I think I found a table with some numbers but I cannot find it anymore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2020 09:35:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045419#M6837</guid>
      <dc:creator>rmelizalde</dc:creator>
      <dc:date>2020-07-30T09:35:03Z</dc:date>
    </item>
    <item>
      <title>Re: VLPS to RUN delay</title>
      <link>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045420#M6838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ricardo, you can find the numbers in the datasheet as below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109012i26D612F8CEBB3EC5/image-size/large?v=v2&amp;amp;px=999" title="vlps to run time.png" alt="vlps to run time.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2020 12:58:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045420#M6838</guid>
      <dc:creator>Jeremy_He</dc:creator>
      <dc:date>2020-07-30T12:58:13Z</dc:date>
    </item>
    <item>
      <title>Re: VLPS to RUN delay</title>
      <link>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045421#M6839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeremy He,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, we are meassuring a delay of 500us from the PORT falling edge, which is the wakeup event, until the associated ISR is serviced.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be going on here? Maybe the system PLL is taking long to lock? Or what?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help or hint would be really appreciated. Because this makes no sense. Why the datasheet states max 17us but we can measure more than 500us.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2020 22:04:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045421#M6839</guid>
      <dc:creator>rmelizalde</dc:creator>
      <dc:date>2020-07-30T22:04:01Z</dc:date>
    </item>
    <item>
      <title>Re: VLPS to RUN delay</title>
      <link>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045422#M6840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ricardo, I tested with a project using S32K144, The time from GPIO wake up to ISR toggle another pin is around 17 us, which matches the datasheet. Please check your code maybe something else is wrong.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the below oscilloscope, Channel 3 is connected to the button SW2(PTC12), Channel 2 is connected to BLUE LED(PTD0) which toggled in PORT ISR after waking up from VLPS. Please check the attached project.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109095i3DDC7775DC269E70/image-size/large?v=v2&amp;amp;px=999" title="VLPS to RUN ISR  timing 17us.jpg" alt="VLPS to RUN ISR  timing 17us.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jul 2020 08:01:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045422#M6840</guid>
      <dc:creator>Jeremy_He</dc:creator>
      <dc:date>2020-07-31T08:01:25Z</dc:date>
    </item>
    <item>
      <title>Re: VLPS to RUN delay</title>
      <link>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045423#M6841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ricardo,&lt;/P&gt;&lt;P&gt;One possible reason could be a delay caused by Digital filter on that port.&lt;/P&gt;&lt;P&gt;Could you scope the active edge along with&amp;nbsp;BUS_CLK on a CLKOUT pin?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109134iCA28F5C9FF1DE56B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jul 2020 08:02:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045423#M6841</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-07-31T08:02:01Z</dc:date>
    </item>
    <item>
      <title>Re: VLPS to RUN delay</title>
      <link>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045424#M6842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can confirm that:&lt;/P&gt;&lt;P&gt;- When RUN mode clock is SPLL and when going to VLPS, then the wakeup time from VLPS to RUN is more than 500us.&lt;/P&gt;&lt;P&gt;- When RUN mode clock is FIRC, when going to VLPS, then the wakeup time from VLPS to RUN is around 10us, as stated in the datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, it seems that waking up when the system clock is SPLL is much slower than with FIRC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please confirm our observations?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why is this difference? Is this the time to lock the SPLL? Is this delay described in the datasheet or the RM?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Aug 2020 07:47:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045424#M6842</guid>
      <dc:creator>rmelizalde</dc:creator>
      <dc:date>2020-08-03T07:47:25Z</dc:date>
    </item>
    <item>
      <title>Re: VLPS to RUN delay</title>
      <link>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045425#M6843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ricardo,&lt;/P&gt;&lt;P&gt;No matter you use SPLL or FIRC as the system clock, the time from VLPS to wakeup PORT ISR shouldn't be affected. The ISR will always be executed before the clock initializing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also in the attached project, the system clock will switch to SPLL_CLK. And a clock out pin(PTE10) that connects to the bus clock is used to show the clock initialing procedure. You can test with the code directly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109514i1D9EF71F4D01785D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109555iDA1EAF066CD2935D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109597iC274EAC81653164A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109556i2C7C2139A093CA91/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.jpg" alt="pastedImage_4.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best wishes.&lt;/P&gt;&lt;P&gt;Jeremy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2020 02:09:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045425#M6843</guid>
      <dc:creator>Jeremy_He</dc:creator>
      <dc:date>2020-08-05T02:09:08Z</dc:date>
    </item>
    <item>
      <title>Re: VLPS to RUN delay</title>
      <link>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045426#M6844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ricardo,&lt;/P&gt;&lt;P&gt;The system clock cannot be derived from FIRC/SPLL when the MCU enters VLPS.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109480iA527E3EAC4B2CF14/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The Power Manager SDK driver switches the clock to SIRC in the Power_SYS_Setmode(VLPS, ...) function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2020 13:23:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/VLPS-to-RUN-delay/m-p/1045426#M6844</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-08-05T13:23:09Z</dc:date>
    </item>
  </channel>
</rss>