<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: s32k qspi read in S32K</title>
    <link>https://community.nxp.com/t5/S32K/s32k-qspi-read/m-p/1042676#M6782</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Daniel&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 May 2020 19:15:41 GMT</pubDate>
    <dc:creator>erdoganguler</dc:creator>
    <dc:date>2020-05-12T19:15:41Z</dc:date>
    <item>
      <title>s32k qspi read</title>
      <link>https://community.nxp.com/t5/S32K/s32k-qspi-read/m-p/1042674#M6780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to read data from flash without waiting. I mean, for example I have 512 Byte circular buffer and first I will read data from flash and put them there. After than i will start working on data. When I work on buffer[127], I want to take 128 byte data from flash and put them buffer[0 -125] and in that time keep working on buffer[127-255]. And when I work on buffer[255], I want to take 128 byte data from flash and put them buffer[127 -255]&amp;nbsp; I dont want to lose time for waiting flash status to be not busy.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can i set up this situation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2020 08:27:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k-qspi-read/m-p/1042674#M6780</guid>
      <dc:creator>erdoganguler</dc:creator>
      <dc:date>2020-05-05T08:27:02Z</dc:date>
    </item>
    <item>
      <title>Re: s32k qspi read</title>
      <link>https://community.nxp.com/t5/S32K/s32k-qspi-read/m-p/1042675#M6781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/erdoganguler"&gt;erdoganguler&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;You can refer to the flash_mx25l6433f1 SDK driver.&lt;/P&gt;&lt;P&gt;There is also this qspi_external_flash_s32k148 example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;FLASH_MX25L6433F_DRV_Read() function does not block the CPU.&lt;/P&gt;&lt;P&gt;You can be working on the previously read data while&amp;nbsp;another read operation is in progress.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is taken from the SDK documentation of the driver located in the SDK installation directory:&lt;/P&gt;&lt;P&gt;.../NXP/S32DS_ARM_v2.2/S32DS/software/S32SDK_S32K1xx_RTM_3.0.0/doc/html_S32K148/group__flash__mx25l6433f__drv.html&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39465iEA5B38601B54830D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 May 2020 09:03:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k-qspi-read/m-p/1042675#M6781</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-05-07T09:03:00Z</dc:date>
    </item>
    <item>
      <title>Re: s32k qspi read</title>
      <link>https://community.nxp.com/t5/S32K/s32k-qspi-read/m-p/1042676#M6782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Daniel&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2020 19:15:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k-qspi-read/m-p/1042676#M6782</guid>
      <dc:creator>erdoganguler</dc:creator>
      <dc:date>2020-05-12T19:15:41Z</dc:date>
    </item>
  </channel>
</rss>