<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K146EVB: How does the UART flow control work for the OpenSDA USB?</title>
    <link>https://community.nxp.com/t5/S32K/S32K146EVB-How-does-the-UART-flow-control-work-for-the-OpenSDA/m-p/1041557#M6754</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is probably more of a general configuration issue than a EVB issue. I am using the S32K146EVB and UART1 (which is connected on the OpenSDA USB port). On Windows 10, I am able to open the virtual COM port and send data to the EVB over UART and received data as well. However, I have now tried the same software on a different PC which happens to be running Windows 7 instead and the terminal no longer receives the UART data sent by the EVB.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The terminal I use on the PC is RealTerm. I am still able to open the COM port and send data to the EVB. I can debug the program and I see that the EVB receives the data and at least attempts to send the response. However, no data is received by the terminal. I tried re-installing the PEMicro drivers to see if that changed anything but it did not. The only difference I have noticed between the Windows 10 and Windows 7 environments is in the hardware flow control detected by RealTerm. When I open the COM port in Windows 10, it shows that the CTS, DCD, and DSR pins are all asserted. However, when I open the COM port in Windows 7, only the CTS pin is asserted. All of these pins are input flow control from the device to the PC, so I don't understand why they would be different between the 2 environments.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What could the issue be?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jul 2020 20:45:40 GMT</pubDate>
    <dc:creator>mikesfn</dc:creator>
    <dc:date>2020-07-13T20:45:40Z</dc:date>
    <item>
      <title>S32K146EVB: How does the UART flow control work for the OpenSDA USB?</title>
      <link>https://community.nxp.com/t5/S32K/S32K146EVB-How-does-the-UART-flow-control-work-for-the-OpenSDA/m-p/1041557#M6754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is probably more of a general configuration issue than a EVB issue. I am using the S32K146EVB and UART1 (which is connected on the OpenSDA USB port). On Windows 10, I am able to open the virtual COM port and send data to the EVB over UART and received data as well. However, I have now tried the same software on a different PC which happens to be running Windows 7 instead and the terminal no longer receives the UART data sent by the EVB.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The terminal I use on the PC is RealTerm. I am still able to open the COM port and send data to the EVB. I can debug the program and I see that the EVB receives the data and at least attempts to send the response. However, no data is received by the terminal. I tried re-installing the PEMicro drivers to see if that changed anything but it did not. The only difference I have noticed between the Windows 10 and Windows 7 environments is in the hardware flow control detected by RealTerm. When I open the COM port in Windows 10, it shows that the CTS, DCD, and DSR pins are all asserted. However, when I open the COM port in Windows 7, only the CTS pin is asserted. All of these pins are input flow control from the device to the PC, so I don't understand why they would be different between the 2 environments.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What could the issue be?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jul 2020 20:45:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146EVB-How-does-the-UART-flow-control-work-for-the-OpenSDA/m-p/1041557#M6754</guid>
      <dc:creator>mikesfn</dc:creator>
      <dc:date>2020-07-13T20:45:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146EVB: How does the UART flow control work for the OpenSDA USB?</title>
      <link>https://community.nxp.com/t5/S32K/S32K146EVB-How-does-the-UART-flow-control-work-for-the-OpenSDA/m-p/1041558#M6755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As an addendum: I have scoped the RXD and TXD pins (PTC6 and 7 for LPUART1 on the EVB) and I can see clearly that the RS-232 data is being received and transmitted on LPUART1, but for some reason the data transmitted by the EVB is not received by the PC.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jul 2020 21:46:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146EVB-How-does-the-UART-flow-control-work-for-the-OpenSDA/m-p/1041558#M6755</guid>
      <dc:creator>mikesfn</dc:creator>
      <dc:date>2020-07-13T21:46:21Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146EVB: How does the UART flow control work for the OpenSDA USB?</title>
      <link>https://community.nxp.com/t5/S32K/S32K146EVB-How-does-the-UART-flow-control-work-for-the-OpenSDA/m-p/1041559#M6756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tried to reinstall the Realterm?&lt;/P&gt;&lt;P&gt;I would like to suggest trying to use another terminal, for example, Tera Term to check if the issue is not in the terminal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2020 09:46:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146EVB-How-does-the-UART-flow-control-work-for-the-OpenSDA/m-p/1041559#M6756</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2020-07-15T09:46:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146EVB: How does the UART flow control work for the OpenSDA USB?</title>
      <link>https://community.nxp.com/t5/S32K/S32K146EVB-How-does-the-UART-flow-control-work-for-the-OpenSDA/m-p/1041560#M6757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have tried several other serial monitors on the same PC with no luck. I tried a few other PCs, and it works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue appears to be something specific to the Windows COM port drivers on this one PC, like some security setting that is blocking Rx flow control. I will have to dig deeper, but as this is not a problem with the OpenSDA firmware as I initially suspected I will close the topic.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2020 20:11:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146EVB-How-does-the-UART-flow-control-work-for-the-OpenSDA/m-p/1041560#M6757</guid>
      <dc:creator>mikesfn</dc:creator>
      <dc:date>2020-07-21T20:11:03Z</dc:date>
    </item>
  </channel>
</rss>