<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K116 Firmware Upgrade in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K116-Firmware-Upgrade/m-p/1032928#M6545</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am currently looking at S32K116 series MCU, would like to know the firmware upgrade via UART.&lt;/P&gt;&lt;P&gt;So for the UART, do I need to connect&amp;nbsp;two lines (Rx,Tx) only or 4 lines with flow control?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Dec 2019 02:46:58 GMT</pubDate>
    <dc:creator>geokpeng_tan</dc:creator>
    <dc:date>2019-12-11T02:46:58Z</dc:date>
    <item>
      <title>S32K116 Firmware Upgrade</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-Firmware-Upgrade/m-p/1032928#M6545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am currently looking at S32K116 series MCU, would like to know the firmware upgrade via UART.&lt;/P&gt;&lt;P&gt;So for the UART, do I need to connect&amp;nbsp;two lines (Rx,Tx) only or 4 lines with flow control?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2019 02:46:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-Firmware-Upgrade/m-p/1032928#M6545</guid>
      <dc:creator>geokpeng_tan</dc:creator>
      <dc:date>2019-12-11T02:46:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32K116 Firmware Upgrade</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-Firmware-Upgrade/m-p/1032929#M6546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to recommend you AN12218 S32K1xx Serial Bootloader&amp;nbsp;with SW located on this link in the Application note section&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mcus/s32k-scalable-microcontrollers-for-automotive-general-purpose-and-and-high-reliability-industrial:S32K?&amp;amp;tab=Documentation_Tab" title="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mcus/s32k-scalable-microcontrollers-for-automotive-general-purpose-and-and-high-reliability-industrial:S32K?&amp;amp;tab=Documentation_Tab"&gt;32-bit Automotive General Purpose MCUs | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hardware flow control is supported but it depends on your application requirements. You do not have to use it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Dec 2019 14:45:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-Firmware-Upgrade/m-p/1032929#M6546</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2019-12-16T14:45:50Z</dc:date>
    </item>
  </channel>
</rss>