<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックECC ERROR</title>
    <link>https://community.nxp.com/t5/S32K/ECC-ERROR/m-p/1031563#M6530</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;My target is S32K148 ,&lt;/P&gt;&lt;P&gt;someone recommends that to avoid setting the ECC error bit , the whole RAM (all of the available RAM, needs to be initialized at&amp;nbsp;every start up).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is that true?&lt;/P&gt;&lt;P&gt;how about FLASH ECC ?&lt;/P&gt;&lt;P&gt;to avoid setting flash ECC , what do I need to do , may be the fact that I'm programming flash will prevent the ECC error?&lt;/P&gt;&lt;P&gt;I know having a CRC and or MAC is a solution but I'm specifically curios about FALSH ECC error?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Dec 2019 19:31:46 GMT</pubDate>
    <dc:creator>hajianik</dc:creator>
    <dc:date>2019-12-10T19:31:46Z</dc:date>
    <item>
      <title>ECC ERROR</title>
      <link>https://community.nxp.com/t5/S32K/ECC-ERROR/m-p/1031563#M6530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;My target is S32K148 ,&lt;/P&gt;&lt;P&gt;someone recommends that to avoid setting the ECC error bit , the whole RAM (all of the available RAM, needs to be initialized at&amp;nbsp;every start up).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is that true?&lt;/P&gt;&lt;P&gt;how about FLASH ECC ?&lt;/P&gt;&lt;P&gt;to avoid setting flash ECC , what do I need to do , may be the fact that I'm programming flash will prevent the ECC error?&lt;/P&gt;&lt;P&gt;I know having a CRC and or MAC is a solution but I'm specifically curios about FALSH ECC error?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Dec 2019 19:31:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ECC-ERROR/m-p/1031563#M6530</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2019-12-10T19:31:46Z</dc:date>
    </item>
    <item>
      <title>Re: ECC ERROR</title>
      <link>https://community.nxp.com/t5/S32K/ECC-ERROR/m-p/1031564#M6531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Koorosh,&lt;/P&gt;&lt;P&gt;SRAM ECC code is generated on RAM writes.&lt;BR /&gt;Out of POR, the SRAM content including the ECC code is not defined.&lt;BR /&gt;You should therefore avoid reading RAM data before they are initialized, the ECC error detection/correction is enabled on SRAM out of reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When a Flash phrase is erased, the corresponding Flash ECC code is also erased (all 1s) which is valid state, it can be read.&lt;BR /&gt;The ECC code is generated and programmed along with the Flash data during programming.&lt;BR /&gt;There are the following Flash commands that can be used to verify that the Flash is correctly erased or programmed:&lt;BR /&gt;Read 1s Block, Read 1s Section, Read 1s All Blocks, Program Check&lt;BR /&gt;S32K1xx RM rev.11 Section 36.5.10 Margin read commands.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2019 10:04:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ECC-ERROR/m-p/1031564#M6531</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-12-11T10:04:42Z</dc:date>
    </item>
  </channel>
</rss>