<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Unable to debug S32K148 using PEmicro Multilink</title>
    <link>https://community.nxp.com/t5/S32K/Unable-to-debug-S32K148-using-PEmicro-Multilink/m-p/1031131#M6502</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/avulamallikarjun@bfusa.com"&gt;avulamallikarjun@bfusa.com&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;The parts are shipped blank, therefore, it is expected that the MCU will be in a periodic reset due to core lockups when powered. But this should not be an issue.&lt;/P&gt;&lt;P&gt;Are there any HW differences between the EVB and your prototype?&lt;/P&gt;&lt;P&gt;Do you have&amp;nbsp;more prototype? Please check all connections and reheat the MCU.&lt;/P&gt;&lt;P&gt;Could you measure the VDD power supply and the PTA5 reset_b pin with an oscilloscope?&lt;/P&gt;&lt;P&gt;Is the reset pin constantly low or is it being triggered periodically?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jan 2020 12:47:35 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2020-01-22T12:47:35Z</dc:date>
    <item>
      <title>Unable to debug S32K148 using PEmicro Multilink</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-debug-S32K148-using-PEmicro-Multilink/m-p/1031130#M6501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working on a prototype&amp;nbsp;board with just S32K148 MCU along with a programming header to flash and debug code. What I have noticed is that upon powering the board, the RESET line always stays low. Due to this, I'm unable to flash code onto the MCU from S32DS by using a Multilink Universal FX debuggger probe from PEmicro where I get the following dialog:&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96897iE54A9E574FCC3C1F/image-size/large?v=v2&amp;amp;px=999" title="no-device-available.png" alt="no-device-available.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It appears to me that the MCU is somehow constantly in RESET mode. I've tried using the Kinetis Recovery Utility but to no avail. I also tried to do a mass erase by selecting the appropriate option from the Debugger configuration of the IDE and that didn't seem to work either. From a hardware design standpoint, I followed the design guidelines document from NXP for S32K1xx devices. Therefore, I'm fairly confident that this may not be a hardware issue. However, I'm able to flash and debug the code on a S32K148 Evaluation Board with no issues at all. This makes me think if it has something to do when dealing with a blank MCU.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Jan 2020 00:04:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-debug-S32K148-using-PEmicro-Multilink/m-p/1031130#M6501</guid>
      <dc:creator>avulamallikarju</dc:creator>
      <dc:date>2020-01-18T00:04:27Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to debug S32K148 using PEmicro Multilink</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-debug-S32K148-using-PEmicro-Multilink/m-p/1031131#M6502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/avulamallikarjun@bfusa.com"&gt;avulamallikarjun@bfusa.com&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;The parts are shipped blank, therefore, it is expected that the MCU will be in a periodic reset due to core lockups when powered. But this should not be an issue.&lt;/P&gt;&lt;P&gt;Are there any HW differences between the EVB and your prototype?&lt;/P&gt;&lt;P&gt;Do you have&amp;nbsp;more prototype? Please check all connections and reheat the MCU.&lt;/P&gt;&lt;P&gt;Could you measure the VDD power supply and the PTA5 reset_b pin with an oscilloscope?&lt;/P&gt;&lt;P&gt;Is the reset pin constantly low or is it being triggered periodically?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2020 12:47:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-debug-S32K148-using-PEmicro-Multilink/m-p/1031131#M6502</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-01-22T12:47:35Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to debug S32K148 using PEmicro Multilink</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-debug-S32K148-using-PEmicro-Multilink/m-p/1031132#M6503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the response. The schematic of my target board is mostly&amp;nbsp;similar to that of the EVB. However, in order to eliminate the variables in this issue, I'm using a different prototype board which has just the MCU populated (plus crystal and other necessary passives). In spite of trying on multiple prototypes, the RESET line stays constantly low&amp;nbsp;whereas Vdd is rock solid at 3.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2020 15:01:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-debug-S32K148-using-PEmicro-Multilink/m-p/1031132#M6503</guid>
      <dc:creator>avulamallikarju</dc:creator>
      <dc:date>2020-01-22T15:01:47Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to debug S32K148 using PEmicro Multilink</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-debug-S32K148-using-PEmicro-Multilink/m-p/1031133#M6504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Daniel,&lt;/P&gt;&lt;P&gt;I believe our HW engineer may have identified the issue. VDDA, VREFH and VREFL were found to be floating. In a different thread in the forums, it has been pointed out that this might cause the RESET line to be constantly low.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2020 15:59:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-debug-S32K148-using-PEmicro-Multilink/m-p/1031133#M6504</guid>
      <dc:creator>avulamallikarju</dc:creator>
      <dc:date>2020-01-22T15:59:05Z</dc:date>
    </item>
  </channel>
</rss>