<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K144UFVLL FLEXIO_UART</title>
    <link>https://community.nxp.com/t5/S32K/S32K144UFVLL-FLEXIO-UART/m-p/1028444#M6439</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/729621187@qq.com"&gt;729621187@qq.com&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;What are the masksets of the two parts? 0N77P, ON74T, ON57U. &lt;BR /&gt;But based on the part numbers, both parts (S32K144UFVLL, S32K144UAVLL) support FlexIO and since it is working on the EVB, I reckon there is a HW issue.&lt;BR /&gt;Do you scope the pins? &lt;BR /&gt;Do you use SDK drivers? &lt;BR /&gt;If so, which version and what is the status returned by each function?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Dec 2019 12:28:13 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2019-12-12T12:28:13Z</dc:date>
    <item>
      <title>S32K144UFVLL FLEXIO_UART</title>
      <link>https://community.nxp.com/t5/S32K/S32K144UFVLL-FLEXIO-UART/m-p/1028443#M6438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I use the flexio_uart of S32K144UFVLL,the data can't send out;but the same code running in demo board of S32K144UAVLL can send data.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Dec 2019 09:10:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144UFVLL-FLEXIO-UART/m-p/1028443#M6438</guid>
      <dc:creator>729621187</dc:creator>
      <dc:date>2019-12-10T09:10:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144UFVLL FLEXIO_UART</title>
      <link>https://community.nxp.com/t5/S32K/S32K144UFVLL-FLEXIO-UART/m-p/1028444#M6439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/729621187@qq.com"&gt;729621187@qq.com&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;What are the masksets of the two parts? 0N77P, ON74T, ON57U. &lt;BR /&gt;But based on the part numbers, both parts (S32K144UFVLL, S32K144UAVLL) support FlexIO and since it is working on the EVB, I reckon there is a HW issue.&lt;BR /&gt;Do you scope the pins? &lt;BR /&gt;Do you use SDK drivers? &lt;BR /&gt;If so, which version and what is the status returned by each function?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Dec 2019 12:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144UFVLL-FLEXIO-UART/m-p/1028444#M6439</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-12-12T12:28:13Z</dc:date>
    </item>
  </channel>
</rss>