<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Comparation between chips in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Comparation-between-chips/m-p/1026980#M6400</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastian Wozniak&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you saw the first line is the ordering information. The second line is the Mask, which is the revision of the silicon. and the third line is the date code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Also I want to ask if there is possible that speed of this two chips can be different even that they have the same Quartz?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;If both chips have the same mask, they have the same silicon revision and then they have the same behavior in hardware. This could be due to changes in the hardware of the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Nov 2019 22:05:27 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2019-11-12T22:05:27Z</dc:date>
    <item>
      <title>Comparation between chips</title>
      <link>https://community.nxp.com/t5/S32K/Comparation-between-chips/m-p/1026979#M6399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to ask what are the differences between those chips:&lt;/P&gt;&lt;P&gt;PS32K148UAVLQ 0N20V QAE1727D&amp;nbsp;&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;FS23K148UJVLQ 0N20V QAY1913X&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found information about first line in S32K DS point 3.2 "Ordering information" but I want to know rest of this code. Could you provide me that, please?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also I want to ask if there is possible that speed of this two chips can be different even that they have the same Quartz?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sebastian Wozniak&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Nov 2019 15:52:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Comparation-between-chips/m-p/1026979#M6399</guid>
      <dc:creator>sebastian_wozni</dc:creator>
      <dc:date>2019-11-08T15:52:10Z</dc:date>
    </item>
    <item>
      <title>Re: Comparation between chips</title>
      <link>https://community.nxp.com/t5/S32K/Comparation-between-chips/m-p/1026980#M6400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastian Wozniak&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you saw the first line is the ordering information. The second line is the Mask, which is the revision of the silicon. and the third line is the date code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Also I want to ask if there is possible that speed of this two chips can be different even that they have the same Quartz?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;If both chips have the same mask, they have the same silicon revision and then they have the same behavior in hardware. This could be due to changes in the hardware of the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Nov 2019 22:05:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Comparation-between-chips/m-p/1026980#M6400</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-11-12T22:05:27Z</dc:date>
    </item>
  </channel>
</rss>