<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Errors creating a LIN Description file through S32DS</title>
    <link>https://community.nxp.com/t5/S32K/Errors-creating-a-LIN-Description-file-through-S32DS/m-p/1025991#M6379</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;as per feedback from LIN Stack expert this is not possible, see below...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;As the J2602 Spec the Error signal must be 3 bit&amp;nbsp; and will be in all of slave transmission frame with offset 5. So we cannot do it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="LIN stack 1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/104276i8EC9A6189E01DF70/image-size/large?v=v2&amp;amp;px=999" role="button" title="LIN stack 1.jpg" alt="LIN stack 1.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Mar 2020 12:56:49 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2020-03-30T12:56:49Z</dc:date>
    <item>
      <title>Errors creating a LIN Description file through S32DS</title>
      <link>https://community.nxp.com/t5/S32K/Errors-creating-a-LIN-Description-file-through-S32DS/m-p/1025990#M6378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the following question:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to configure a Lin_Stack application project, I'm configuring it to use LIN J2602. In the component inspector window, when I configure the frames that will be sent/received, the S32DS eventually shows me that, for each slave node, there should be a response error signal (which fits well with my configuration).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="LIN_ISSUE.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103798i0E6C191BA6A9D942/image-size/large?v=v2&amp;amp;px=999" role="button" title="LIN_ISSUE.PNG" alt="LIN_ISSUE.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the signal which is the response error in my LIN description file is not 3 bits long, as the configuration requires. I have a signal that will be in charge of carrying the response errors, but it is&amp;nbsp;8 bits long since it will carry other data as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="LIN_ISSUE_2.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103875i4157DF8ACAFF567C/image-size/large?v=v2&amp;amp;px=999" role="button" title="LIN_ISSUE_2.PNG" alt="LIN_ISSUE_2.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I try to add a signal which is not 3 bits long to the Response Error field, it gets cleared automatically. Also, if my signal is 3 bits long but doesn't have a 5-bit offset, I also get an error which shows that response errors must have a 5-bit offset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="LIN_ISSUE_3.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103998i15E01B99ED0F34AD/image-size/large?v=v2&amp;amp;px=999" role="button" title="LIN_ISSUE_3.PNG" alt="LIN_ISSUE_3.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to set up my configuration without errors and make the S32DS recognize an 8 bit long signal as the response error signal?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2020 20:49:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Errors-creating-a-LIN-Description-file-through-S32DS/m-p/1025990#M6378</guid>
      <dc:creator>joseponc</dc:creator>
      <dc:date>2020-03-26T20:49:50Z</dc:date>
    </item>
    <item>
      <title>Re: Errors creating a LIN Description file through S32DS</title>
      <link>https://community.nxp.com/t5/S32K/Errors-creating-a-LIN-Description-file-through-S32DS/m-p/1025991#M6379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;as per feedback from LIN Stack expert this is not possible, see below...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;As the J2602 Spec the Error signal must be 3 bit&amp;nbsp; and will be in all of slave transmission frame with offset 5. So we cannot do it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="LIN stack 1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/104276i8EC9A6189E01DF70/image-size/large?v=v2&amp;amp;px=999" role="button" title="LIN stack 1.jpg" alt="LIN stack 1.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2020 12:56:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Errors-creating-a-LIN-Description-file-through-S32DS/m-p/1025991#M6379</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-03-30T12:56:49Z</dc:date>
    </item>
  </channel>
</rss>