<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックDebugging while using external power</title>
    <link>https://community.nxp.com/t5/S32K/Debugging-while-using-external-power/m-p/1025766#M6376</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using a S32K116 board. Can I debug using USB Open-SDA interface while powering from a 12V external source? I know that I need to change J107 to position 1-2, but I don't know if the USB will short with the externa power.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Nov 2019 17:48:49 GMT</pubDate>
    <dc:creator>rjmalmeida0</dc:creator>
    <dc:date>2019-11-08T17:48:49Z</dc:date>
    <item>
      <title>Debugging while using external power</title>
      <link>https://community.nxp.com/t5/S32K/Debugging-while-using-external-power/m-p/1025766#M6376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using a S32K116 board. Can I debug using USB Open-SDA interface while powering from a 12V external source? I know that I need to change J107 to position 1-2, but I don't know if the USB will short with the externa power.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Nov 2019 17:48:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Debugging-while-using-external-power/m-p/1025766#M6376</guid>
      <dc:creator>rjmalmeida0</dc:creator>
      <dc:date>2019-11-08T17:48:49Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging while using external power</title>
      <link>https://community.nxp.com/t5/S32K/Debugging-while-using-external-power/m-p/1025767#M6377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;Rui Almeida,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, it is possible to debug with the on-board debugger while powering from a 12V external source. As you mentioned, you only need to change the position of J107 to 1-2 and connect the external power source and the USB cable. &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2019 18:23:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Debugging-while-using-external-power/m-p/1025767#M6377</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2019-11-13T18:23:16Z</dc:date>
    </item>
  </channel>
</rss>