<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Not able to flash using OpenSDA</title>
    <link>https://community.nxp.com/t5/S32K/Not-able-to-flash-using-OpenSDA/m-p/1021066#M6285</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anoop,&lt;/P&gt;&lt;P&gt;Can you share the project?&lt;/P&gt;&lt;P&gt;Do you have any other debugger?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Mar 2020 09:29:02 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2020-03-18T09:29:02Z</dc:date>
    <item>
      <title>Not able to flash using OpenSDA</title>
      <link>https://community.nxp.com/t5/S32K/Not-able-to-flash-using-OpenSDA/m-p/1021065#M6284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;Iam using s32k144 evaluation board. After flashing an application related to watchdog Iam not able to debug the board using openSDA again. OpenSDA LED(D2) is OFF, LED(D3) is ON and the RESET LED(D1) is continuously ON. Also it is not able to detect the port for the interface(OpenSDA) used. Also Iam not able to enter the bootloader mode. Kindly suggest me&amp;nbsp; a solution to recover the board..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Anoop&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2020 14:16:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Not-able-to-flash-using-OpenSDA/m-p/1021065#M6284</guid>
      <dc:creator>anoop_radhakris</dc:creator>
      <dc:date>2020-03-12T14:16:03Z</dc:date>
    </item>
    <item>
      <title>Re: Not able to flash using OpenSDA</title>
      <link>https://community.nxp.com/t5/S32K/Not-able-to-flash-using-OpenSDA/m-p/1021066#M6285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anoop,&lt;/P&gt;&lt;P&gt;Can you share the project?&lt;/P&gt;&lt;P&gt;Do you have any other debugger?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 09:29:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Not-able-to-flash-using-OpenSDA/m-p/1021066#M6285</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-03-18T09:29:02Z</dc:date>
    </item>
  </channel>
</rss>