<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 PDB trigger input source</title>
    <link>https://community.nxp.com/t5/S32K/PDB-trigger-input-source/m-p/1020451#M6280</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all, I have a question about the external trigger source for PDB-ADC peripheral.&lt;/P&gt;&lt;P&gt;At pag. 1182 of S32K manual, I read:&lt;/P&gt;&lt;P&gt;"...A trigger input event is defined as a rising edge being detected on a selected&lt;BR /&gt;trigger input source…."&lt;/P&gt;&lt;P&gt;I would like to know if there is the possibility to generate a trigger also when a falling edge is detecte.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jan 2020 16:02:56 GMT</pubDate>
    <dc:creator>anita_tranzillo</dc:creator>
    <dc:date>2020-01-16T16:02:56Z</dc:date>
    <item>
      <title>PDB trigger input source</title>
      <link>https://community.nxp.com/t5/S32K/PDB-trigger-input-source/m-p/1020451#M6280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all, I have a question about the external trigger source for PDB-ADC peripheral.&lt;/P&gt;&lt;P&gt;At pag. 1182 of S32K manual, I read:&lt;/P&gt;&lt;P&gt;"...A trigger input event is defined as a rising edge being detected on a selected&lt;BR /&gt;trigger input source…."&lt;/P&gt;&lt;P&gt;I would like to know if there is the possibility to generate a trigger also when a falling edge is detecte.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jan 2020 16:02:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/PDB-trigger-input-source/m-p/1020451#M6280</guid>
      <dc:creator>anita_tranzillo</dc:creator>
      <dc:date>2020-01-16T16:02:56Z</dc:date>
    </item>
    <item>
      <title>Re: PDB trigger input source</title>
      <link>https://community.nxp.com/t5/S32K/PDB-trigger-input-source/m-p/1020452#M6281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi anita tranzillo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately, in the section 44.4.1 PDB pre-trigger and trigger outputs only explains how to use the rising edge and in the registers doesn't explain how to change the polarity.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jan 2020 23:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/PDB-trigger-input-source/m-p/1020452#M6281</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-01-20T23:44:34Z</dc:date>
    </item>
  </channel>
</rss>