<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Enabling FPU on S32K144 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Enabling-FPU-on-S32K144/m-p/664002#M627</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Goodmorning, i need to enable the FPU on S32K144.&lt;/P&gt;&lt;P&gt;How can i do that?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I&amp;nbsp;need to compute such function with logaritmics operation using float variables.&lt;BR /&gt;After activation&amp;nbsp;must i&amp;nbsp;use some special function to use FPU or is it automatic?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Feb 2017 10:58:02 GMT</pubDate>
    <dc:creator>pietroserao</dc:creator>
    <dc:date>2017-02-02T10:58:02Z</dc:date>
    <item>
      <title>Enabling FPU on S32K144</title>
      <link>https://community.nxp.com/t5/S32K/Enabling-FPU-on-S32K144/m-p/664002#M627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Goodmorning, i need to enable the FPU on S32K144.&lt;/P&gt;&lt;P&gt;How can i do that?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I&amp;nbsp;need to compute such function with logaritmics operation using float variables.&lt;BR /&gt;After activation&amp;nbsp;must i&amp;nbsp;use some special function to use FPU or is it automatic?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Feb 2017 10:58:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Enabling-FPU-on-S32K144/m-p/664002#M627</guid>
      <dc:creator>pietroserao</dc:creator>
      <dc:date>2017-02-02T10:58:02Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling FPU on S32K144</title>
      <link>https://community.nxp.com/t5/S32K/Enabling-FPU-on-S32K144/m-p/664003#M628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FPU activation is done automatically based on the toolchain settings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For S32 Design Studio:&lt;/P&gt;&lt;P&gt;Right click on the project and select &lt;STRONG&gt;Properties.&amp;nbsp;&lt;/STRONG&gt;The following window will appear:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12678iD23AAE048ACF168C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this window:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;1) Go to &lt;STRONG&gt;C/C++ build&lt;/STRONG&gt; (1)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;2) Select &lt;STRONG&gt;Settings&lt;/STRONG&gt; (2)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;3) From there select&amp;nbsp;&lt;STRONG&gt;Target Processor &lt;/STRONG&gt;(3)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;4) Configure&amp;nbsp;&lt;STRONG&gt;Float ABI &lt;/STRONG&gt;and&lt;STRONG&gt; FPU Type&amp;nbsp;&lt;/STRONG&gt;to &lt;EM&gt;FP instructions(hard) &lt;/EM&gt;and &lt;EM&gt;fpv4-sp-d16 &lt;/EM&gt;(4).&lt;/P&gt;&lt;P&gt;Click on ok and then rebuild the project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need the procedure for FPU activation for different toolchains or IDE please let me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Rares&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Feb 2017 11:45:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Enabling-FPU-on-S32K144/m-p/664003#M628</guid>
      <dc:creator>raresvasile</dc:creator>
      <dc:date>2017-02-02T11:45:46Z</dc:date>
    </item>
  </channel>
</rss>