<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Flash reliability S32K146</title>
    <link>https://community.nxp.com/t5/S32K/Flash-reliability-S32K146/m-p/1019355#M6264</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Eduard&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;This is the only specification available, min 1k cycles guaranteed&amp;nbsp;across product temperature specification in Normal Mode (Table 25, footnote 2).&lt;/P&gt;&lt;P&gt;It is not the maximum number of cycles but the minimum number of cycles guaranteed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 Jan 2020 12:44:30 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2020-01-31T12:44:30Z</dc:date>
    <item>
      <title>Flash reliability S32K146</title>
      <link>https://community.nxp.com/t5/S32K/Flash-reliability-S32K146/m-p/1019354#M6263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sr/ Mdm,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using S32K146 and as per datasheet requirements:&lt;/P&gt;&lt;P&gt;NVM reliability specifications when using as Program and Data Flash (attached picture):&lt;/P&gt;&lt;P&gt;nnvmcycp Cycling endurance 1 K — — cycles 2, 3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does it mean that the maximum number of cycles per each Sector that NXP guarantee for this uC is 1K?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;If we do more than 1K reflashing in a cycle test of code reflashing (same sectors), NXP doesn't guarantee the flash reliability after the 1K reflash? Even if&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;reflash is done&amp;nbsp;in a cycle test, thus, all of them during 1day?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance and best regards,&lt;/P&gt;&lt;P&gt;Eduard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jan 2020 07:57:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flash-reliability-S32K146/m-p/1019354#M6263</guid>
      <dc:creator>eduard_reina</dc:creator>
      <dc:date>2020-01-30T07:57:27Z</dc:date>
    </item>
    <item>
      <title>Re: Flash reliability S32K146</title>
      <link>https://community.nxp.com/t5/S32K/Flash-reliability-S32K146/m-p/1019355#M6264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Eduard&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;This is the only specification available, min 1k cycles guaranteed&amp;nbsp;across product temperature specification in Normal Mode (Table 25, footnote 2).&lt;/P&gt;&lt;P&gt;It is not the maximum number of cycles but the minimum number of cycles guaranteed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jan 2020 12:44:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flash-reliability-S32K146/m-p/1019355#M6264</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-01-31T12:44:30Z</dc:date>
    </item>
  </channel>
</rss>