<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Program partition command</title>
    <link>https://community.nxp.com/t5/S32K/Program-partition-command/m-p/1017831#M6229</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all, when I read mannual chapter 36.5.11.14 Program Partition command, has the following comment:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CAUTION&lt;/P&gt;&lt;P&gt;While different partitions of the FlexNVM are available, the intention is that a single partition choice is used throughout the entire lifetime of a given application. The FlexNVM Partition Code choices affect the endurance and data retention characteristics of the device .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what's the meaning of this this passage?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Dec 2019 11:57:56 GMT</pubDate>
    <dc:creator>814420552</dc:creator>
    <dc:date>2019-12-06T11:57:56Z</dc:date>
    <item>
      <title>Program partition command</title>
      <link>https://community.nxp.com/t5/S32K/Program-partition-command/m-p/1017831#M6229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all, when I read mannual chapter 36.5.11.14 Program Partition command, has the following comment:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CAUTION&lt;/P&gt;&lt;P&gt;While different partitions of the FlexNVM are available, the intention is that a single partition choice is used throughout the entire lifetime of a given application. The FlexNVM Partition Code choices affect the endurance and data retention characteristics of the device .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what's the meaning of this this passage?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Dec 2019 11:57:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Program-partition-command/m-p/1017831#M6229</guid>
      <dc:creator>814420552</dc:creator>
      <dc:date>2019-12-06T11:57:56Z</dc:date>
    </item>
    <item>
      <title>Re: Program partition command</title>
      <link>https://community.nxp.com/t5/S32K/Program-partition-command/m-p/1017832#M6230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Within the FlexNVM you have different partitions (data flash, emulated EEPROM, etc.), however, to increase the&amp;nbsp;endurance and data retention characteristics of the device it's recommended that you use only a single partition.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Victor&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Dec 2019 23:02:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Program-partition-command/m-p/1017832#M6230</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2019-12-10T23:02:01Z</dc:date>
    </item>
  </channel>
</rss>