<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Short circuit, Freedom board S32 K144</title>
    <link>https://community.nxp.com/t5/S32K/Short-circuit-Freedom-board-S32-K144/m-p/600804#M62</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it's not really clear to me what happened. I would try to measure all the supply pins, reset pin and so on to see if there's something unusual...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Mar 2017 08:15:13 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2017-03-06T08:15:13Z</dc:date>
    <item>
      <title>Short circuit, Freedom board S32 K144</title>
      <link>https://community.nxp.com/t5/S32K/Short-circuit-Freedom-board-S32-K144/m-p/600803#M61</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an issue with FRDMPK 144 Q100 freedom board. Unfortunately because of a short circuit the board is not responding.&lt;/P&gt;&lt;P&gt;The short circuit was on a&amp;nbsp;GPIO pin which was in Input mode.&lt;/P&gt;&lt;P&gt;I cannot flash a program.(i can paste .srec file to the board drive but there is no response) the text message in the board drive showing the last status was "Error 7".&lt;/P&gt;&lt;P&gt;I am not sure what it is.&lt;/P&gt;&lt;P&gt;I loaded the SDA file again in bootloader mode and then the status changed to "Ready" but the board is not responding.&lt;/P&gt;&lt;P&gt;Debugging using S32 design studio is throwing an error saying "error occured while connecting to the interface".&lt;/P&gt;&lt;P&gt;Does this mean the board is completely damaged? or is there any other way to work around.?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking forward to your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Nirmal Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2017 10:49:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Short-circuit-Freedom-board-S32-K144/m-p/600803#M61</guid>
      <dc:creator>nirmalthomas</dc:creator>
      <dc:date>2017-02-27T10:49:21Z</dc:date>
    </item>
    <item>
      <title>Re: Short circuit, Freedom board S32 K144</title>
      <link>https://community.nxp.com/t5/S32K/Short-circuit-Freedom-board-S32-K144/m-p/600804#M62</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it's not really clear to me what happened. I would try to measure all the supply pins, reset pin and so on to see if there's something unusual...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Mar 2017 08:15:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Short-circuit-Freedom-board-S32-K144/m-p/600804#M62</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2017-03-06T08:15:13Z</dc:date>
    </item>
  </channel>
</rss>