<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic questions about example project for spi  in S32K</title>
    <link>https://community.nxp.com/t5/S32K/questions-about-example-project-for-spi/m-p/1016634#M6197</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Dear expert&lt;/SPAN&gt;，&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I used S32K144 EVM board , and the SDK version is S32SDK_S32K1xx_RTM_3.0.0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The example lpspi_transfer work abnormally.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The EVB power is 12V, and I connect the PTB4 (output of mater spi_0) with PTD1(input of slave spi_1), and PTE1(input of master spi_0) with PTD2(output of slave spi_1). &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;slaveDataSend, masterDataReceive, masterDataSend, slaveDataReceive are initialized as 0x00.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But after the ADC voltage is sampled, the slaveDataSend is 0xc3, but masterDataReceive is 0ff. When slaveDataSend changes as ADC voltage, but the masterDataReceive is always 0xff.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It means the master SPI can not receive correctly. What may be the reason? Could you help me&lt;/SPAN&gt;？&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you very much!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Feb 2020 02:00:19 GMT</pubDate>
    <dc:creator>zhaoyanling</dc:creator>
    <dc:date>2020-02-26T02:00:19Z</dc:date>
    <item>
      <title>questions about example project for spi</title>
      <link>https://community.nxp.com/t5/S32K/questions-about-example-project-for-spi/m-p/1016634#M6197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Dear expert&lt;/SPAN&gt;，&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I used S32K144 EVM board , and the SDK version is S32SDK_S32K1xx_RTM_3.0.0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The example lpspi_transfer work abnormally.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The EVB power is 12V, and I connect the PTB4 (output of mater spi_0) with PTD1(input of slave spi_1), and PTE1(input of master spi_0) with PTD2(output of slave spi_1). &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;slaveDataSend, masterDataReceive, masterDataSend, slaveDataReceive are initialized as 0x00.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But after the ADC voltage is sampled, the slaveDataSend is 0xc3, but masterDataReceive is 0ff. When slaveDataSend changes as ADC voltage, but the masterDataReceive is always 0xff.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It means the master SPI can not receive correctly. What may be the reason? Could you help me&lt;/SPAN&gt;？&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you very much!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2020 02:00:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/questions-about-example-project-for-spi/m-p/1016634#M6197</guid>
      <dc:creator>zhaoyanling</dc:creator>
      <dc:date>2020-02-26T02:00:19Z</dc:date>
    </item>
    <item>
      <title>Re: questions about example project for spi</title>
      <link>https://community.nxp.com/t5/S32K/questions-about-example-project-for-spi/m-p/1016635#M6198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/zhaoyanling@bhap.com.cn"&gt;zhaoyanling@bhap.com.cn&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;I just tested the&amp;nbsp;lpspi_transfer_s32K144 SDK example (RTM 3.0.2, S32DS for ARM 2.2)&lt;/P&gt;&lt;P&gt;And it seems that the&amp;nbsp;pin wiring description in main.c does not match the actual PIN configuration.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/99218iF101AD6A0C0C5BCF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/99258i3F036DFD431B0714/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Please connect PTB2 to PTB14.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 12:20:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/questions-about-example-project-for-spi/m-p/1016635#M6198</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-02-27T12:20:58Z</dc:date>
    </item>
    <item>
      <title>Re: questions about example project for spi</title>
      <link>https://community.nxp.com/t5/S32K/questions-about-example-project-for-spi/m-p/1016636#M6199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo Deniel,&lt;/P&gt;&lt;P&gt;I tried as your suggestion. It works.&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;Best Regards.Wish you happy!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2020 02:06:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/questions-about-example-project-for-spi/m-p/1016636#M6199</guid>
      <dc:creator>zhaoyanling</dc:creator>
      <dc:date>2020-02-28T02:06:25Z</dc:date>
    </item>
  </channel>
</rss>