<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 LPUART receive function not working (LPUART_DRV_ReceiveData) with SDK 3.0.0</title>
    <link>https://community.nxp.com/t5/S32K/LPUART-receive-function-not-working-LPUART-DRV-ReceiveData-with/m-p/1015948#M6193</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks Diana Batriova for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Feature:Porting of sdk 0.8.6 echo example(without processor expert) to&lt;/P&gt;&lt;P&gt;sdk 3.0.0(with processor expert) Serial communication with LPUART&lt;/P&gt;&lt;P&gt;Scenario: echo testing with LPUART&lt;/P&gt;&lt;P&gt;Given:start up code initialization done,&lt;/P&gt;&lt;P&gt;Given: clock configuration is done&lt;/P&gt;&lt;P&gt;Given: LPUART2 initialization done,&lt;/P&gt;&lt;P&gt;When:trying to transmit(using LPUART_DRV_SendData) it is able to&lt;/P&gt;&lt;P&gt;receive in terminal.&lt;/P&gt;&lt;P&gt;and trying to receive data(using LPUART_DRV_ReceiveData) from terminal&lt;/P&gt;&lt;P&gt;Then:device should receive.&lt;/P&gt;&lt;P&gt;Observation: Device is unable to receive data.&lt;/P&gt;&lt;P&gt;Indiviual sdk example are working fine.But when Iam trying to use&lt;/P&gt;&lt;P&gt;LPUART echo example code from sdk 0.8.6(without processor expert) to&lt;/P&gt;&lt;P&gt;sdk 3.0.0(with processor expert),receive(LPUART_DRV_ReceiveData)is not&lt;/P&gt;&lt;P&gt;working for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Nov 2019 06:35:42 GMT</pubDate>
    <dc:creator>anoop_radhakris</dc:creator>
    <dc:date>2019-11-07T06:35:42Z</dc:date>
    <item>
      <title>LPUART receive function not working (LPUART_DRV_ReceiveData) with SDK 3.0.0</title>
      <link>https://community.nxp.com/t5/S32K/LPUART-receive-function-not-working-LPUART-DRV-ReceiveData-with/m-p/1015948#M6193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks Diana Batriova for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Feature:Porting of sdk 0.8.6 echo example(without processor expert) to&lt;/P&gt;&lt;P&gt;sdk 3.0.0(with processor expert) Serial communication with LPUART&lt;/P&gt;&lt;P&gt;Scenario: echo testing with LPUART&lt;/P&gt;&lt;P&gt;Given:start up code initialization done,&lt;/P&gt;&lt;P&gt;Given: clock configuration is done&lt;/P&gt;&lt;P&gt;Given: LPUART2 initialization done,&lt;/P&gt;&lt;P&gt;When:trying to transmit(using LPUART_DRV_SendData) it is able to&lt;/P&gt;&lt;P&gt;receive in terminal.&lt;/P&gt;&lt;P&gt;and trying to receive data(using LPUART_DRV_ReceiveData) from terminal&lt;/P&gt;&lt;P&gt;Then:device should receive.&lt;/P&gt;&lt;P&gt;Observation: Device is unable to receive data.&lt;/P&gt;&lt;P&gt;Indiviual sdk example are working fine.But when Iam trying to use&lt;/P&gt;&lt;P&gt;LPUART echo example code from sdk 0.8.6(without processor expert) to&lt;/P&gt;&lt;P&gt;sdk 3.0.0(with processor expert),receive(LPUART_DRV_ReceiveData)is not&lt;/P&gt;&lt;P&gt;working for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Nov 2019 06:35:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPUART-receive-function-not-working-LPUART-DRV-ReceiveData-with/m-p/1015948#M6193</guid>
      <dc:creator>anoop_radhakris</dc:creator>
      <dc:date>2019-11-07T06:35:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPUART receive function not working (LPUART_DRV_ReceiveData) with SDK 3.0.0</title>
      <link>https://community.nxp.com/t5/S32K/LPUART-receive-function-not-working-LPUART-DRV-ReceiveData-with/m-p/1015949#M6194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anoop,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are welcome.&lt;/P&gt;&lt;P&gt;I would like to recommend you to use directly the&amp;nbsp;&lt;STRONG&gt;lpuart_echo_s32k144&lt;/STRONG&gt; SDK 3.0.0 example from S32 Design Studio for ARM 2018.R1. File -&amp;gt; New -&amp;gt; Project from Example :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92359i58368C3B5706FB6B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After that, you don't need to port anything. The older versions don't have to be compatible.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2019 09:37:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPUART-receive-function-not-working-LPUART-DRV-ReceiveData-with/m-p/1015949#M6194</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2019-11-13T09:37:42Z</dc:date>
    </item>
  </channel>
</rss>