<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ENET MII no Rx in S32K</title>
    <link>https://community.nxp.com/t5/S32K/ENET-MII-no-Rx/m-p/1014346#M6168</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you still have the issue? If yes, kindly share with us the ETH and PORT configuration, better in xdm or epc, so we can see if your configuration has something incorrect or not.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Mar 2020 09:04:12 GMT</pubDate>
    <dc:creator>namnguyenviet</dc:creator>
    <dc:date>2020-03-24T09:04:12Z</dc:date>
    <item>
      <title>ENET MII no Rx</title>
      <link>https://community.nxp.com/t5/S32K/ENET-MII-no-Rx/m-p/1014345#M6167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Integrated Vector Ethernet stack for Autosar.&lt;/P&gt;&lt;P&gt;Micro: S32K148&lt;/P&gt;&lt;P&gt;Transceiver: Marvell 88Q1010&lt;/P&gt;&lt;P&gt;Interface between PHY and MAC is MII.&lt;/P&gt;&lt;P&gt;During packet transmission no Rx interrupt on ENET, but Tx interrupt is there.&lt;/P&gt;&lt;P&gt;Checked the MII Rx and RX_DV lines.Seems signals present in these lines when data are transmitting from PHY to MAC.But no interrupt on MAC.Also all statistics register values are zeros for Rx.&lt;BR /&gt;Also when trying to send packet from MAC to PHY via Eth_Transmit(), data is transmitting via Tx lines and it is receiving on PHY and received on test PC via Media converter board. ie Tx lines are working.&lt;BR /&gt;But for Rx MAC not receiving any frames from PHY.&lt;/P&gt;&lt;DIV style="color: black; background-color: #ffffff; border: 0px; font-size: 12pt;"&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Nov 2019 06:52:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ENET-MII-no-Rx/m-p/1014345#M6167</guid>
      <dc:creator>jithin_m</dc:creator>
      <dc:date>2019-11-20T06:52:05Z</dc:date>
    </item>
    <item>
      <title>Re: ENET MII no Rx</title>
      <link>https://community.nxp.com/t5/S32K/ENET-MII-no-Rx/m-p/1014346#M6168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you still have the issue? If yes, kindly share with us the ETH and PORT configuration, better in xdm or epc, so we can see if your configuration has something incorrect or not.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2020 09:04:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ENET-MII-no-Rx/m-p/1014346#M6168</guid>
      <dc:creator>namnguyenviet</dc:creator>
      <dc:date>2020-03-24T09:04:12Z</dc:date>
    </item>
  </channel>
</rss>