<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: [S32K3] about LVD Interrupt</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-about-LVD-Interrupt/m-p/2420832#M61459</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A voltage of 5V is being applied to the following pins:&lt;/P&gt;&lt;P&gt;Using a 100-pin MCU (FS32K312NHT0VPAST)&lt;/P&gt;&lt;P&gt;VREFH: PIN 8&lt;BR /&gt;VDD_HV_A: PIN 10&lt;BR /&gt;VDD_HV_A-2: PIN 37&lt;BR /&gt;VDD_HV_A-3: PIN 62&lt;BR /&gt;VDD_HV_A-4: PIN 87&lt;/P&gt;&lt;P&gt;Although 5V is supplied, the LVD5AF flag register keeps being set.&lt;BR /&gt;Are there any additional points or registers I should check?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BRs,&lt;/P&gt;&lt;P&gt;Sean&lt;/P&gt;</description>
    <pubDate>Tue, 13 Oct 2026 23:55:49 GMT</pubDate>
    <dc:creator>ssean</dc:creator>
    <dc:date>2026-10-13T23:55:49Z</dc:date>
    <item>
      <title>[S32K3] about LVD Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-about-LVD-Interrupt/m-p/2420571#M61451</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to use the LVD interrupt feature on the S32K3 MCU.&lt;/P&gt;&lt;P&gt;I set LVDIEEnable = true in the MCU configuration.&lt;BR /&gt;Although 5V is currently supplied to the MCU, Power_Ip_PMC_VoltageErrorIsr() keeps being triggered continuously.&lt;BR /&gt;I would like to ask if this is normal behavior, or if I have misconfigured something.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ssean_0-1791874212868.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/397864iB1464554C5C83F33/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ssean_0-1791874212868.png" alt="ssean_0-1791874212868.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ssean_1-1791874253693.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/397865i5702FAD1185E5847/image-size/large?v=v2&amp;amp;px=999" role="button" title="ssean_1-1791874253693.png" alt="ssean_1-1791874253693.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ssean_2-1791874284581.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/397866i68264B7D16A52802/image-size/large?v=v2&amp;amp;px=999" role="button" title="ssean_2-1791874284581.png" alt="ssean_2-1791874284581.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2026 06:51:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-about-LVD-Interrupt/m-p/2420571#M61451</guid>
      <dc:creator>ssean</dc:creator>
      <dc:date>2026-10-13T06:51:45Z</dc:date>
    </item>
    <item>
      <title>Re: [S32K3] about LVD Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-about-LVD-Interrupt/m-p/2420708#M61454</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/215656"&gt;@ssean&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;If LVD5AF stays set after you clear it.&lt;/P&gt;
&lt;P&gt;The voltage must be lower than the specified threshold:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1791887685044.png" style="width: 745px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/397881i138A920037E993D9/image-dimensions/745x118?v=v2" width="745" height="118" role="button" title="danielmartynek_0-1791887685044.png" alt="danielmartynek_0-1791887685044.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Can you measure the voltage?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2026 10:44:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-about-LVD-Interrupt/m-p/2420708#M61454</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-10-13T10:44:25Z</dc:date>
    </item>
    <item>
      <title>Re: [S32K3] about LVD Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-about-LVD-Interrupt/m-p/2420832#M61459</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A voltage of 5V is being applied to the following pins:&lt;/P&gt;&lt;P&gt;Using a 100-pin MCU (FS32K312NHT0VPAST)&lt;/P&gt;&lt;P&gt;VREFH: PIN 8&lt;BR /&gt;VDD_HV_A: PIN 10&lt;BR /&gt;VDD_HV_A-2: PIN 37&lt;BR /&gt;VDD_HV_A-3: PIN 62&lt;BR /&gt;VDD_HV_A-4: PIN 87&lt;/P&gt;&lt;P&gt;Although 5V is supplied, the LVD5AF flag register keeps being set.&lt;BR /&gt;Are there any additional points or registers I should check?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BRs,&lt;/P&gt;&lt;P&gt;Sean&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2026 23:55:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-about-LVD-Interrupt/m-p/2420832#M61459</guid>
      <dc:creator>ssean</dc:creator>
      <dc:date>2026-10-13T23:55:49Z</dc:date>
    </item>
    <item>
      <title>Re: [S32K3] about LVD Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-about-LVD-Interrupt/m-p/2421068#M61463</link>
      <description>&lt;P&gt;Can you please specif the part number?&lt;/P&gt;
&lt;P&gt;Which RTD revision do you use?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 14 Oct 2026 11:13:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-about-LVD-Interrupt/m-p/2421068#M61463</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-10-14T11:13:34Z</dc:date>
    </item>
    <item>
      <title>Re: [S32K3] about LVD Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-about-LVD-Interrupt/m-p/2422437#M61542</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am currently using RTD 4.0.0 HF04.&lt;BR /&gt;I identified a few errors in the RTD code as well as an issue in my configuration.&lt;BR /&gt;After making the necessary adjustments, I confirmed that the interrupt is triggered properly at the LVD voltage level.&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BRs,&lt;/P&gt;&lt;P&gt;Sean Sung&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2026 23:18:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-about-LVD-Interrupt/m-p/2422437#M61542</guid>
      <dc:creator>ssean</dc:creator>
      <dc:date>2026-10-20T23:18:28Z</dc:date>
    </item>
  </channel>
</rss>