<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is it possible to simultaneously use EEPROM (with backup) from bootloader placed in FlexNVM? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Is-it-possible-to-simultaneously-use-EEPROM-with-backup-from/m-p/1011634#M6141</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/bhav97"&gt;bhav97&lt;/A&gt;,&lt;BR /&gt;Yes, you would not be able to execute EEPROM writes (2) and SCEc commands (3) from DFlash.&lt;BR /&gt;You should be able to use Strict Sequential Boot Mode (1) while the core stays in RESET. &lt;BR /&gt;But the secure boot is run on PFLASH block starting at address 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Nov 2019 09:49:23 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2019-11-25T09:49:23Z</dc:date>
    <item>
      <title>Is it possible to simultaneously use EEPROM (with backup) from bootloader placed in FlexNVM?</title>
      <link>https://community.nxp.com/t5/S32K/Is-it-possible-to-simultaneously-use-EEPROM-with-backup-from/m-p/1011633#M6140</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to achieve a configuration in which I plan to use the following features on a S32K118&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.) EEPROM emulation with size set to 2kB&lt;/P&gt;&lt;P&gt;2.) DEPART set to 1001 to use 24kB of FlexNVM as EEPROM backup and 8 kB as DFLASH&lt;/P&gt;&lt;P&gt;3.) CSec enabled with 3 keys&lt;/P&gt;&lt;P&gt;4.) 256 kB of PFlash is used by the application code&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reference manual mentions the possibility of loading code into the FlexNVM section, however Section 5 of AN12003.pdf (Using S32K148 FlexNVM Memory) says&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;SPAN style="left: 134.177px; top: 933.941px; font-size: 15px; font-family: sans-serif; transform: scaleX(1.01844);"&gt;Any software driver that uses CSEc, EEPROM (writes only) or Flash controller commands must not be placed in&lt;/SPAN&gt;&lt;SPAN style="left: 148.352px; top: 953.941px; font-size: 15px; font-family: sans-serif; transform: scaleX(1.02754);"&gt;FlexNVM’s PFlash.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;In the event that my bootloader is placed in the FlexNVM,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1.) will I lose the secure boot options?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2.) will I lose the ability to write to EEPROM (in the bootloader code)?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;3.) will I lose the ability to perform CSec operations (in the bootloasder code)?&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2019 14:22:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-it-possible-to-simultaneously-use-EEPROM-with-backup-from/m-p/1011633#M6140</guid>
      <dc:creator>bhav97</dc:creator>
      <dc:date>2019-11-19T14:22:59Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to simultaneously use EEPROM (with backup) from bootloader placed in FlexNVM?</title>
      <link>https://community.nxp.com/t5/S32K/Is-it-possible-to-simultaneously-use-EEPROM-with-backup-from/m-p/1011634#M6141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/bhav97"&gt;bhav97&lt;/A&gt;,&lt;BR /&gt;Yes, you would not be able to execute EEPROM writes (2) and SCEc commands (3) from DFlash.&lt;BR /&gt;You should be able to use Strict Sequential Boot Mode (1) while the core stays in RESET. &lt;BR /&gt;But the secure boot is run on PFLASH block starting at address 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Nov 2019 09:49:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-it-possible-to-simultaneously-use-EEPROM-with-backup-from/m-p/1011634#M6141</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-11-25T09:49:23Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to simultaneously use EEPROM (with backup) from bootloader placed in FlexNVM?</title>
      <link>https://community.nxp.com/t5/S32K/Is-it-possible-to-simultaneously-use-EEPROM-with-backup-from/m-p/1011635#M6142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the clarifications. I will proceed accordingly&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2019 05:52:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-it-possible-to-simultaneously-use-EEPROM-with-backup-from/m-p/1011635#M6142</guid>
      <dc:creator>bhav97</dc:creator>
      <dc:date>2019-11-26T05:52:13Z</dc:date>
    </item>
  </channel>
</rss>