<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Regarding Flash Programming for the FRDM-A-S32K144N</title>
    <link>https://community.nxp.com/t5/S32K/Regarding-Flash-Programming-for-the-FRDM-A-S32K144N/m-p/2417306#M61254</link>
    <description>&lt;P&gt;Hi&amp;nbsp;Fukuda,&lt;/P&gt;
&lt;P&gt;I don't have the newly released FRDM-A-S32K144N development board on hand, so I haven't tested it myself. If you aren't in a rush, I can help you troubleshoot the issue now, and then perform tests on my end once I receive the board—which I expect to arrive in mid-October.&lt;/P&gt;
&lt;P&gt;After plugging the cable into the &lt;STRONG&gt;J1&lt;/STRONG&gt; USB Type-C port, please take a photo of the top side of the board and share it with me.&lt;BR /&gt;I am not sure which two LEDs you are referring to, as the SPF-96556_B.pdf document only lists &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;D5&lt;/STRONG&gt; &lt;/FONT&gt;(Red) and &lt;FONT color="#FF6600"&gt;&lt;STRONG&gt;D4&lt;/STRONG&gt; &lt;/FONT&gt;(Orange).&lt;BR /&gt;If &lt;FONT color="#FF6600"&gt;&lt;STRONG&gt;D4&lt;/STRONG&gt; &lt;/FONT&gt;is lit, it indicates that the onboard &lt;STRONG&gt;OpenSDA&lt;/STRONG&gt; debugger is functioning correctly. However, if &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;D5&lt;/STRONG&gt; &lt;/FONT&gt;is lit, it indicates that the S32K144N is in a reset state (The &lt;STRONG&gt;RESET_MCU&lt;/STRONG&gt; signal may go low); please use an oscilloscope to observe the signal and check for the frequency of periodic low pulses.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Additionally, I am unsure what program was previously flashed onto the &lt;STRONG&gt;S32K144N&lt;/STRONG&gt;. If it is a blank chip and the &lt;STRONG&gt;RESET_MCU&lt;/STRONG&gt; signal shows periodic high-level pulses with a period of ~118µs, you can recover the MCU by executing a "mass erase" command via the SWD/JTAG debug interface.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Since the onboard debugger is provided by PEMicro, it is recommended to download the latest "&lt;/SPAN&gt;&lt;A href="https://www.pemicro.com/downloads/download_file.cfm?download_id=346" target="_blank" rel="noopener"&gt;USB Multilink Resources Installer&lt;/A&gt;&lt;SPAN&gt;" from the "Support &amp;amp; Downloads" category of the "&lt;/SPAN&gt;&lt;A href="https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320180" target="_blank" rel="noopener"&gt;Multilink Debug Probes&lt;/A&gt;&lt;SPAN&gt;". After installation, open &lt;/SPAN&gt;&lt;EM&gt;&lt;STRONG&gt;PEFirmwareConfig.exe&lt;/STRONG&gt;&lt;/EM&gt;&lt;SPAN&gt; located in C:\PEMicro\Multilink_Resources to check the firmware version.&amp;nbsp;&lt;/SPAN&gt;Select Hardware Type: &lt;STRONG&gt;Multilink ACP Embedded - OnBoard ARM Debug Interface&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;Then, check for available updates.&lt;/P&gt;
&lt;P&gt;It appears you have already refer to the discussion "&lt;A href="https://community.nxp.com/t5/S32K/S32K144-D2-RED-LED-is-ON-always/m-p/1567621" target="_self"&gt;S32K144 D2 RED LED is ON always&lt;/A&gt;". Please note that the &lt;STRONG&gt;Kinetis_Recovery_Utility&lt;/STRONG&gt; (Version &lt;STRONG&gt;8.17&lt;/STRONG&gt;) previously provided on the PEMicro website did not work correctly; the &lt;STRONG&gt;Kinetis_Recovery_Utility&lt;/STRONG&gt; (Version &lt;STRONG&gt;1.06&lt;/STRONG&gt;)—which I uploaded as an attachment in that discussion—works properly.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;When using the &lt;STRONG&gt;Kinetis_Recovery_Utility&lt;/STRONG&gt;, It is recommended to keep the PEMicro debugger powered on and repeatedly power-cycle reset only the S32K chip.&lt;BR /&gt;If you have an external debugger like the &lt;STRONG&gt;Multilink &lt;/STRONG&gt;connected to the &lt;STRONG&gt;J3&lt;/STRONG&gt;, you can repeatedly plug and unplug &lt;STRONG&gt;J1&lt;/STRONG&gt; to cycle power to the &lt;STRONG&gt;S32K144N&lt;/STRONG&gt; while keeping the external &lt;STRONG&gt;Multilink&lt;/STRONG&gt;&amp;nbsp;active.&lt;BR /&gt;However, if you do not have an external &lt;STRONG&gt;Multilink&lt;/STRONG&gt; and are relying solely on the onboard &lt;STRONG&gt;OpenSDA&lt;/STRONG&gt; debugger, the design of the &lt;STRONG&gt;FRDM-A-S32K144N&lt;/STRONG&gt; presents some inconvenience. Jumper &lt;STRONG&gt;SJ10&lt;/STRONG&gt; is not as convenient as &lt;STRONG&gt;J107&lt;/STRONG&gt; on the &lt;STRONG&gt;S32K144EVB&lt;/STRONG&gt; for repeatedly cycling power to the S32K144. I am not certain whether repeatedly pressing &lt;STRONG&gt;SW2&lt;/STRONG&gt; alone would allow the &lt;STRONG&gt;Kinetis_Recovery_Utility&lt;/STRONG&gt; to successfully halt the S32K144N at the right moment.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
    <pubDate>Wed, 30 Sep 2026 04:20:40 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2026-09-30T04:20:40Z</dc:date>
    <item>
      <title>Regarding Flash Programming for the FRDM-A-S32K144N</title>
      <link>https://community.nxp.com/t5/S32K/Regarding-Flash-Programming-for-the-FRDM-A-S32K144N/m-p/2416785#M61221</link>
      <description>&lt;P&gt;I was debugging using the FRDM-A-S32K144N when the following symptoms occurred:&lt;/P&gt;&lt;P&gt;* Unable to write to flash memory.&lt;BR /&gt;* Since the write failure, the power LED and reset LED have remained constantly lit.&lt;/P&gt;&lt;P&gt;I attempted recovery by performing the following steps:&lt;/P&gt;&lt;P&gt;1. Tried writing to the flash memory by unplugging and replugging the USB cable while holding down the reset button, aiming to catch the window before the infinite loop started.&lt;BR /&gt;* Attempted this dozens of times but was unsuccessful.&lt;/P&gt;&lt;P&gt;2. Connected the USB cable while holding down the reset button to enter bootloader mode.&lt;BR /&gt;* Flashed "BOOTUPDATEAPP_Pemicro_v111.SDA".&lt;BR /&gt;* Then flashed "MSD-DEBUG-EVB-S32K144_PEmicro_v125.SDA".&lt;BR /&gt;* The situation did not improve.&lt;/P&gt;&lt;P&gt;3. Attempted flash recovery using "Kinetis_Recovery_Utility.exe".&lt;BR /&gt;* Unplugged and replugged the USB cable several times, but the process did not complete.&lt;/P&gt;&lt;P&gt;I am unsure what to try next.&lt;BR /&gt;If anyone knows how to restore the board, could you please advise me on the procedure?&lt;/P&gt;</description>
      <pubDate>Mon, 28 Sep 2026 13:08:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Regarding-Flash-Programming-for-the-FRDM-A-S32K144N/m-p/2416785#M61221</guid>
      <dc:creator>Fukuda</dc:creator>
      <dc:date>2026-09-28T13:08:26Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding Flash Programming for the FRDM-A-S32K144N</title>
      <link>https://community.nxp.com/t5/S32K/Regarding-Flash-Programming-for-the-FRDM-A-S32K144N/m-p/2417306#M61254</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Fukuda,&lt;/P&gt;
&lt;P&gt;I don't have the newly released FRDM-A-S32K144N development board on hand, so I haven't tested it myself. If you aren't in a rush, I can help you troubleshoot the issue now, and then perform tests on my end once I receive the board—which I expect to arrive in mid-October.&lt;/P&gt;
&lt;P&gt;After plugging the cable into the &lt;STRONG&gt;J1&lt;/STRONG&gt; USB Type-C port, please take a photo of the top side of the board and share it with me.&lt;BR /&gt;I am not sure which two LEDs you are referring to, as the SPF-96556_B.pdf document only lists &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;D5&lt;/STRONG&gt; &lt;/FONT&gt;(Red) and &lt;FONT color="#FF6600"&gt;&lt;STRONG&gt;D4&lt;/STRONG&gt; &lt;/FONT&gt;(Orange).&lt;BR /&gt;If &lt;FONT color="#FF6600"&gt;&lt;STRONG&gt;D4&lt;/STRONG&gt; &lt;/FONT&gt;is lit, it indicates that the onboard &lt;STRONG&gt;OpenSDA&lt;/STRONG&gt; debugger is functioning correctly. However, if &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;D5&lt;/STRONG&gt; &lt;/FONT&gt;is lit, it indicates that the S32K144N is in a reset state (The &lt;STRONG&gt;RESET_MCU&lt;/STRONG&gt; signal may go low); please use an oscilloscope to observe the signal and check for the frequency of periodic low pulses.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Additionally, I am unsure what program was previously flashed onto the &lt;STRONG&gt;S32K144N&lt;/STRONG&gt;. If it is a blank chip and the &lt;STRONG&gt;RESET_MCU&lt;/STRONG&gt; signal shows periodic high-level pulses with a period of ~118µs, you can recover the MCU by executing a "mass erase" command via the SWD/JTAG debug interface.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Since the onboard debugger is provided by PEMicro, it is recommended to download the latest "&lt;/SPAN&gt;&lt;A href="https://www.pemicro.com/downloads/download_file.cfm?download_id=346" target="_blank" rel="noopener"&gt;USB Multilink Resources Installer&lt;/A&gt;&lt;SPAN&gt;" from the "Support &amp;amp; Downloads" category of the "&lt;/SPAN&gt;&lt;A href="https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320180" target="_blank" rel="noopener"&gt;Multilink Debug Probes&lt;/A&gt;&lt;SPAN&gt;". After installation, open &lt;/SPAN&gt;&lt;EM&gt;&lt;STRONG&gt;PEFirmwareConfig.exe&lt;/STRONG&gt;&lt;/EM&gt;&lt;SPAN&gt; located in C:\PEMicro\Multilink_Resources to check the firmware version.&amp;nbsp;&lt;/SPAN&gt;Select Hardware Type: &lt;STRONG&gt;Multilink ACP Embedded - OnBoard ARM Debug Interface&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;Then, check for available updates.&lt;/P&gt;
&lt;P&gt;It appears you have already refer to the discussion "&lt;A href="https://community.nxp.com/t5/S32K/S32K144-D2-RED-LED-is-ON-always/m-p/1567621" target="_self"&gt;S32K144 D2 RED LED is ON always&lt;/A&gt;". Please note that the &lt;STRONG&gt;Kinetis_Recovery_Utility&lt;/STRONG&gt; (Version &lt;STRONG&gt;8.17&lt;/STRONG&gt;) previously provided on the PEMicro website did not work correctly; the &lt;STRONG&gt;Kinetis_Recovery_Utility&lt;/STRONG&gt; (Version &lt;STRONG&gt;1.06&lt;/STRONG&gt;)—which I uploaded as an attachment in that discussion—works properly.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;When using the &lt;STRONG&gt;Kinetis_Recovery_Utility&lt;/STRONG&gt;, It is recommended to keep the PEMicro debugger powered on and repeatedly power-cycle reset only the S32K chip.&lt;BR /&gt;If you have an external debugger like the &lt;STRONG&gt;Multilink &lt;/STRONG&gt;connected to the &lt;STRONG&gt;J3&lt;/STRONG&gt;, you can repeatedly plug and unplug &lt;STRONG&gt;J1&lt;/STRONG&gt; to cycle power to the &lt;STRONG&gt;S32K144N&lt;/STRONG&gt; while keeping the external &lt;STRONG&gt;Multilink&lt;/STRONG&gt;&amp;nbsp;active.&lt;BR /&gt;However, if you do not have an external &lt;STRONG&gt;Multilink&lt;/STRONG&gt; and are relying solely on the onboard &lt;STRONG&gt;OpenSDA&lt;/STRONG&gt; debugger, the design of the &lt;STRONG&gt;FRDM-A-S32K144N&lt;/STRONG&gt; presents some inconvenience. Jumper &lt;STRONG&gt;SJ10&lt;/STRONG&gt; is not as convenient as &lt;STRONG&gt;J107&lt;/STRONG&gt; on the &lt;STRONG&gt;S32K144EVB&lt;/STRONG&gt; for repeatedly cycling power to the S32K144. I am not certain whether repeatedly pressing &lt;STRONG&gt;SW2&lt;/STRONG&gt; alone would allow the &lt;STRONG&gt;Kinetis_Recovery_Utility&lt;/STRONG&gt; to successfully halt the S32K144N at the right moment.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
      <pubDate>Wed, 30 Sep 2026 04:20:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Regarding-Flash-Programming-for-the-FRDM-A-S32K144N/m-p/2417306#M61254</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2026-09-30T04:20:40Z</dc:date>
    </item>
  </channel>
</rss>