<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックLPIT GPT documentation missing</title>
    <link>https://community.nxp.com/t5/S32K/LPIT-GPT-documentation-missing/m-p/2416134#M61184</link>
    <description>&lt;P&gt;I'd like to use the LPIT GPT functionality of the LPit_Gpt IP driver module.&lt;BR /&gt;The S32K118 example shows various functions regarding this module, like "&lt;SPAN&gt;Lpit_Gpt_Ip_Init&lt;/SPAN&gt;", "&lt;SPAN&gt;Lpit_Gpt_Ip_InitChannel&lt;/SPAN&gt;" or "&lt;SPAN&gt;Lpit_Gpt_Ip_StartTimer&lt;/SPAN&gt;".&lt;BR /&gt;However, when checking the corresponding User Manual or Integration Manual, none of those functions are listed.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Where can I find proper documentation?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;RTD Version is 3.0.0 QLP06.&lt;/P&gt;</description>
    <pubDate>Thu, 24 Sep 2026 13:04:14 GMT</pubDate>
    <dc:creator>daniel_meier</dc:creator>
    <dc:date>2026-09-24T13:04:14Z</dc:date>
    <item>
      <title>LPIT GPT documentation missing</title>
      <link>https://community.nxp.com/t5/S32K/LPIT-GPT-documentation-missing/m-p/2416134#M61184</link>
      <description>&lt;P&gt;I'd like to use the LPIT GPT functionality of the LPit_Gpt IP driver module.&lt;BR /&gt;The S32K118 example shows various functions regarding this module, like "&lt;SPAN&gt;Lpit_Gpt_Ip_Init&lt;/SPAN&gt;", "&lt;SPAN&gt;Lpit_Gpt_Ip_InitChannel&lt;/SPAN&gt;" or "&lt;SPAN&gt;Lpit_Gpt_Ip_StartTimer&lt;/SPAN&gt;".&lt;BR /&gt;However, when checking the corresponding User Manual or Integration Manual, none of those functions are listed.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Where can I find proper documentation?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;RTD Version is 3.0.0 QLP06.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Sep 2026 13:04:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPIT-GPT-documentation-missing/m-p/2416134#M61184</guid>
      <dc:creator>daniel_meier</dc:creator>
      <dc:date>2026-09-24T13:04:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPIT GPT documentation missing</title>
      <link>https://community.nxp.com/t5/S32K/LPIT-GPT-documentation-missing/m-p/2416171#M61186</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/168838"&gt;@daniel_meier&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The User and Integration manuals are mainly describing the&amp;nbsp;AUTOSAR high-level driver functions (which in consequence, use the lower-level functions). If you require further information about the IP lower-level APIs, you can refer to the &lt;STRONG&gt;LPit_Gpt_Ip.h&lt;/STRONG&gt; header.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For example, for&amp;nbsp;&lt;SPAN&gt;&lt;STRONG&gt;Lpit_Gpt_Ip_Init&lt;/STRONG&gt;:&lt;/SPAN&gt;&lt;/P&gt;
&lt;LI-CODE lang="c"&gt;/**
* @brief         Function Name : Lpit_Gpt_Ip_Init
* @details       Driver initialization function for LPit instance.
*
*
* @param[in]     instance     LPIT hw instance number
* @param[in]     config       Pointer to a selected configuration structure
* @return        void
* @pre           The data structure including the configuration set required for initializing the driver
*
*/
void Lpit_Gpt_Ip_Init(uint8 instance, const Lpit_Gpt_Ip_InstanceConfigType *config);&lt;/LI-CODE&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Thu, 24 Sep 2026 17:21:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPIT-GPT-documentation-missing/m-p/2416171#M61186</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2026-09-24T17:21:11Z</dc:date>
    </item>
  </channel>
</rss>