<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32DS S32K358 Project Inquiry in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32DS-S32K358-Project-Inquiry/m-p/2414903#M61124</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263485"&gt;@wj_kwak&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For S32K358, S32DS creates two independent projects by default, one for M7_0 and one for M7_2. These projects correspond to the two processing cores. They do not represent a bootloader area and an application area.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The S32DS project creation wizard does not normally create a single project containing the application for both cores. If such a project structure is required, it has to be created/configured manually. However, in most cases there is no need to do this and the typical approach is to use two independent projects, one for each core.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The "Inherit boot core toolchain" option can be used to inherit the toolchain configuration from the boot-core project when creating the project for the other core. If it is enabled, you can select the toolchain only for Cortex-M7_0_0. The toolchain selection for Cortex-M7_0_2 will be greyed-out because the configuration from the Cortex-M7_0_0 will apply.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can also refer to the multicore examples and documentation provided here:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;community.nxp.com/t5/S32K/S32K324-Multi-Core-Example-Project-based-on-Whiteboard/m-p/1547771&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The package demonstrates both approaches: independent projects for each core and a single project for both cores compiled into a single ELF file.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;So, M7_0 and M7_2 should not be understood as bootloader and application projects. They are simply the projects associated with the respective cores.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Mon, 21 Sep 2026 09:19:01 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2026-09-21T09:19:01Z</dc:date>
    <item>
      <title>S32DS S32K358 Project Inquiry</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-S32K358-Project-Inquiry/m-p/2414673#M61107</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wj_kwak_0-1789777426372.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/396578i266ADE907DC98C68/image-size/medium?v=v2&amp;amp;px=400" role="button" title="wj_kwak_0-1789777426372.png" alt="wj_kwak_0-1789777426372.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a question about creating the S32K358 project.&lt;/P&gt;&lt;P&gt;I am curious why two projects, M7_0 and M7_2, are being created.&lt;/P&gt;&lt;P&gt;I want to know the function of the Inherit boot core toolchain button..&lt;/P&gt;&lt;P&gt;My teammate says that the reference documentation states M7_0 is the bootloader area and M7_2 is the application area, but I haven't been able to verify this in the documentation. I would like to confirm this.&lt;/P&gt;</description>
      <pubDate>Sat, 19 Sep 2026 00:28:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-S32K358-Project-Inquiry/m-p/2414673#M61107</guid>
      <dc:creator>wj_kwak</dc:creator>
      <dc:date>2026-09-19T00:28:10Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS S32K358 Project Inquiry</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-S32K358-Project-Inquiry/m-p/2414903#M61124</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263485"&gt;@wj_kwak&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For S32K358, S32DS creates two independent projects by default, one for M7_0 and one for M7_2. These projects correspond to the two processing cores. They do not represent a bootloader area and an application area.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The S32DS project creation wizard does not normally create a single project containing the application for both cores. If such a project structure is required, it has to be created/configured manually. However, in most cases there is no need to do this and the typical approach is to use two independent projects, one for each core.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The "Inherit boot core toolchain" option can be used to inherit the toolchain configuration from the boot-core project when creating the project for the other core. If it is enabled, you can select the toolchain only for Cortex-M7_0_0. The toolchain selection for Cortex-M7_0_2 will be greyed-out because the configuration from the Cortex-M7_0_0 will apply.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can also refer to the multicore examples and documentation provided here:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;community.nxp.com/t5/S32K/S32K324-Multi-Core-Example-Project-based-on-Whiteboard/m-p/1547771&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The package demonstrates both approaches: independent projects for each core and a single project for both cores compiled into a single ELF file.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;So, M7_0 and M7_2 should not be understood as bootloader and application projects. They are simply the projects associated with the respective cores.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2026 09:19:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-S32K358-Project-Inquiry/m-p/2414903#M61124</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2026-09-21T09:19:01Z</dc:date>
    </item>
  </channel>
</rss>