<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K118 Interrupts in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K118-Interrupts/m-p/2414431#M61081</link>
    <description>&lt;P&gt;You can also get the&amp;nbsp;&lt;SPAN&gt;interrupt examples through installing "S32SDK_S32K1xx_RTM_4.0.2.exe"&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 18 Sep 2026 01:28:48 GMT</pubDate>
    <dc:creator>dadin852</dc:creator>
    <dc:date>2026-09-18T01:28:48Z</dc:date>
    <item>
      <title>S32K118 Interrupts</title>
      <link>https://community.nxp.com/t5/S32K/S32K118-Interrupts/m-p/1853441#M34601</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am triyng to setup an interrupt on LPTI timer or LPTMR0 one.&lt;/P&gt;&lt;P&gt;Both timers are running in the correct way (the end count flags will be settled) but&lt;/P&gt;&lt;P&gt;no way to get the interrupt.&lt;/P&gt;&lt;P&gt;I am using S32K118 evaluation board and S32DS IDE.&lt;/P&gt;&lt;P&gt;Can someone help me?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Apr 2024 12:09:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K118-Interrupts/m-p/1853441#M34601</guid>
      <dc:creator>paolonese</dc:creator>
      <dc:date>2024-04-24T12:09:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32K118 Interrupts</title>
      <link>https://community.nxp.com/t5/S32K/S32K118-Interrupts/m-p/1854568#M34648</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please refer to the LPIT and LPTMR interrupt examples in S32K1 SDK 4.0.3 of S32DS v3.4.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lpit lptmr interrupt S32K1 SDK RTM 4.0.3.png" style="width: 812px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/275822i9D890D25CED44A17/image-size/large?v=v2&amp;amp;px=999" role="button" title="lpit lptmr interrupt S32K1 SDK RTM 4.0.3.png" alt="lpit lptmr interrupt S32K1 SDK RTM 4.0.3.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 25 Apr 2024 08:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K118-Interrupts/m-p/1854568#M34648</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-04-25T08:53:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32K118 Interrupts</title>
      <link>https://community.nxp.com/t5/S32K/S32K118-Interrupts/m-p/2414431#M61081</link>
      <description>&lt;P&gt;You can also get the&amp;nbsp;&lt;SPAN&gt;interrupt examples through installing "S32SDK_S32K1xx_RTM_4.0.2.exe"&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2026 01:28:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K118-Interrupts/m-p/2414431#M61081</guid>
      <dc:creator>dadin852</dc:creator>
      <dc:date>2026-09-18T01:28:48Z</dc:date>
    </item>
  </channel>
</rss>