<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Does NXP official have a code routine for configuring external boot for S32K344 chip? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Does-NXP-official-have-a-code-routine-for-configuring-external/m-p/2413787#M61030</link>
    <description>&lt;P&gt;In a nonsecure boot configuration - does the first bootloader run from ROM (is it immutable)?&lt;/P&gt;&lt;P&gt;Can this first bootloader be configured to boot the subsequent bootloaders/application images from an external source/flash?&lt;/P&gt;</description>
    <pubDate>Tue, 15 Sep 2026 18:24:16 GMT</pubDate>
    <dc:creator>CTCoder1</dc:creator>
    <dc:date>2026-09-15T18:24:16Z</dc:date>
    <item>
      <title>Does NXP official have a code routine for configuring external boot for S32K344 chip?</title>
      <link>https://community.nxp.com/t5/S32K/Does-NXP-official-have-a-code-routine-for-configuring-external/m-p/1852869#M34560</link>
      <description>&lt;P&gt;Does NXP official have a code routine and&amp;nbsp;tutorial for configuring external boot for S32K344 chip? We would like to configure the chip to boot from the SD card？&lt;/P&gt;</description>
      <pubDate>Wed, 24 Apr 2024 00:52:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Does-NXP-official-have-a-code-routine-for-configuring-external/m-p/1852869#M34560</guid>
      <dc:creator>SCoder41</dc:creator>
      <dc:date>2024-04-24T00:52:38Z</dc:date>
    </item>
    <item>
      <title>Re: Does NXP official have a code routine for configuring external boot for S32K344 chip?</title>
      <link>https://community.nxp.com/t5/S32K/Does-NXP-official-have-a-code-routine-for-configuring-external/m-p/1854915#M34674</link>
      <description>&lt;P&gt;This device does not offer an option to boot from external memory.&lt;/P&gt;
&lt;P&gt;Device supports secure and nonsecure boot modes but in both cases it is internal flash boot.&lt;/P&gt;</description>
      <pubDate>Thu, 25 Apr 2024 16:11:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Does-NXP-official-have-a-code-routine-for-configuring-external/m-p/1854915#M34674</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2024-04-25T16:11:58Z</dc:date>
    </item>
    <item>
      <title>Re: Does NXP official have a code routine for configuring external boot for S32K344 chip?</title>
      <link>https://community.nxp.com/t5/S32K/Does-NXP-official-have-a-code-routine-for-configuring-external/m-p/2413787#M61030</link>
      <description>&lt;P&gt;In a nonsecure boot configuration - does the first bootloader run from ROM (is it immutable)?&lt;/P&gt;&lt;P&gt;Can this first bootloader be configured to boot the subsequent bootloaders/application images from an external source/flash?&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2026 18:24:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Does-NXP-official-have-a-code-routine-for-configuring-external/m-p/2413787#M61030</guid>
      <dc:creator>CTCoder1</dc:creator>
      <dc:date>2026-09-15T18:24:16Z</dc:date>
    </item>
  </channel>
</rss>