<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 CAN sample point configure in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-CAN-sample-point-configure/m-p/1010270#M6101</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how did you get a 16tq? With 20MHz protocol clock and desired 500kbps you will need either 8, 10 or 20 tq and also 40tq if CBT register is used. The setting of 80% sample point is possible.&lt;/P&gt;&lt;P&gt;You can try to test below tool for CAN bit calculation.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-342618"&gt;https://community.nxp.com/docs/DOC-342618&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Mar 2020 20:57:52 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2020-03-11T20:57:52Z</dc:date>
    <item>
      <title>S32K144 CAN sample point configure</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-CAN-sample-point-configure/m-p/1010269#M6100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV style="color: #000000; background-color: #ffffff; font-weight: normal; font-size: 16px;"&gt;1. The figure below shows that the sample point I configured is 80%, the crystal vibration on the board is 20MHz, the baud rate is 500K, and the time share of 20tq, which can be configured successfully.&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Catch(03-09-13-4(03-09-13-51-34).jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/97780iC81D52FCDD321D88/image-size/large?v=v2&amp;amp;px=999" role="button" title="Catch(03-09-13-4(03-09-13-51-34).jpg" alt="Catch(03-09-13-4(03-09-13-51-34).jpg" /&gt;&lt;/span&gt;&lt;BR /&gt;2. The current problem is: based on the same 20MHz crystal vibration on the board and the baud rate of 500K, the sampling point should be configured to meet the requirements of 75%~83.4%, but the time share is 16tq, and the configuration is not successful.&lt;BR /&gt;&lt;BR /&gt;How to configure it?Thank you very much!&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Mar 2020 11:04:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-CAN-sample-point-configure/m-p/1010269#M6100</guid>
      <dc:creator>jianguo_li</dc:creator>
      <dc:date>2020-03-10T11:04:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 CAN sample point configure</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-CAN-sample-point-configure/m-p/1010270#M6101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how did you get a 16tq? With 20MHz protocol clock and desired 500kbps you will need either 8, 10 or 20 tq and also 40tq if CBT register is used. The setting of 80% sample point is possible.&lt;/P&gt;&lt;P&gt;You can try to test below tool for CAN bit calculation.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-342618"&gt;https://community.nxp.com/docs/DOC-342618&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Mar 2020 20:57:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-CAN-sample-point-configure/m-p/1010270#M6101</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-03-11T20:57:52Z</dc:date>
    </item>
  </channel>
</rss>