<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K312 Freertos build issue for the FreeRTOS_Toggle_Led_Example_S32K312</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-Freertos-build-issue-for-the-FreeRTOS-Toggle-Led-Example/m-p/2412400#M60955</link>
    <description>&lt;P&gt;Thanks for the quick update the given RTD version is resolved my issue.&lt;/P&gt;</description>
    <pubDate>Wed, 09 Sep 2026 13:20:19 GMT</pubDate>
    <dc:creator>pramodj2</dc:creator>
    <dc:date>2026-09-09T13:20:19Z</dc:date>
    <item>
      <title>S32K312 Freertos build issue for the FreeRTOS_Toggle_Led_Example_S32K312</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-Freertos-build-issue-for-the-FreeRTOS-Toggle-Led-Example/m-p/2412224#M60945</link>
      <description>&lt;DIV&gt;&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I have downloaded the following RTD and FreeRTOS packages from the NXP website:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;SW32K3_RTD_R23-11_7.0.1_P02_D2603_DesignStudio_updatesite.tar&lt;/LI&gt;&lt;LI&gt;SW32K3_FreeRTOS_11.1.0_0.8.0_CD1_D2603_DesignStudio_updatesite.tar&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I am using a Windows system and have successfully imported/opened the &lt;STRONG&gt;FreeRTOS_Toggle_Led_Example_S32K312&lt;/STRONG&gt; project in &lt;STRONG&gt;S32 Design Studio (V3.6.10)&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;However, when I try to build the application, I encounter the error &lt;SPAN&gt;#include "FreeRTOSConfig.h file not found as&amp;nbsp;&lt;/SPAN&gt;shown in the attached screenshot (BE1).&lt;/P&gt;&lt;P&gt;Additionally, when I open the project's &lt;STRONG&gt;.mex&lt;/STRONG&gt; file, Config Tools displays the following error (Refer attached&amp;nbsp;&lt;STRONG&gt;Mex &lt;/STRONG&gt;file)&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;STRONG&gt;"The tool does not support the selected processor."&lt;/STRONG&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Could you please guide me on the following points?&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is there any specific version of &lt;STRONG&gt;S32 Design Studio&lt;/STRONG&gt; required for these RTD and FreeRTOS packages?&lt;/LI&gt;&lt;LI&gt;Are there any additional updates, plugins, or device support packages that need to be installed for &lt;STRONG&gt;S32K312&lt;/STRONG&gt;?&lt;/LI&gt;&lt;LI&gt;What is the correct procedure to build and run the &lt;STRONG&gt;FreeRTOS_Toggle_Led_Example_S32K312&lt;/STRONG&gt; sample application?&lt;/LI&gt;&lt;LI&gt;My end goal is to run FreeRTOS on the &lt;STRONG&gt;S32K312 EVB&lt;/STRONG&gt;. Could you please advise on the recommended setup and installation steps?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;I have attached the build error screenshots (BE1 and Mex) for reference.&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;&lt;STRONG&gt;Pramod Jadhav&lt;/STRONG&gt;&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 09 Sep 2026 05:51:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-Freertos-build-issue-for-the-FreeRTOS-Toggle-Led-Example/m-p/2412224#M60945</guid>
      <dc:creator>pramodj2</dc:creator>
      <dc:date>2026-09-09T05:51:21Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 Freertos build issue for the FreeRTOS_Toggle_Led_Example_S32K312</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-Freertos-build-issue-for-the-FreeRTOS-Toggle-Led-Example/m-p/2412314#M60951</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;the SW32K3_RTD_R23-11_7.0.1_P02_D2603_DesignStudio_updatesite.zip includes just Crypto driver. You need to install based RTD package first before adding FreeRTOS one.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1788946493548.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/396159iF4A35806EDFF981B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PetrS_0-1788946493548.png" alt="PetrS_0-1788946493548.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;PetrS_0-1788946493548.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Once you have RTD &amp;amp; FreeRTOS sucesfully installed, just create new project from example&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_1-1788946542398.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/396160i24315BBEA50CE190/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PetrS_1-1788946542398.png" alt="PetrS_1-1788946542398.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;PetrS_1-1788946542398.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;After it is loaded, open mex file and click on Update Code button. It should add missing drivers etc.&amp;nbsp;&lt;BR /&gt;Then you can Build the demo&lt;BR /&gt;You can also right click on project in Project Explorer window and select Update Code and Build Project.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1788946711279.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/396162iB8DE5008E62FD86B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PetrS_0-1788946711279.png" alt="PetrS_0-1788946711279.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;PetrS_0-1788946711279.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Sep 2026 09:42:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-Freertos-build-issue-for-the-FreeRTOS-Toggle-Led-Example/m-p/2412314#M60951</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2026-09-09T09:42:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 Freertos build issue for the FreeRTOS_Toggle_Led_Example_S32K312</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-Freertos-build-issue-for-the-FreeRTOS-Toggle-Led-Example/m-p/2412400#M60955</link>
      <description>&lt;P&gt;Thanks for the quick update the given RTD version is resolved my issue.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Sep 2026 13:20:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-Freertos-build-issue-for-the-FreeRTOS-Toggle-Led-Example/m-p/2412400#M60955</guid>
      <dc:creator>pramodj2</dc:creator>
      <dc:date>2026-09-09T13:20:19Z</dc:date>
    </item>
  </channel>
</rss>