<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K312 Firmware-Compatibility in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-Firmware-Compatibility/m-p/2410720#M60850</link>
    <description>&lt;P&gt;Hello NXP Support,&lt;/P&gt;&lt;P&gt;We are developing TPMS controllers using S32K312HVS MCUs.&lt;BR /&gt;Currently sourced from China (Rev: 0P09C), we are transitioning to Malaysia production (same MCU model).&lt;/P&gt;&lt;P&gt;For Phase 1 validation, please confirm the following:&lt;/P&gt;&lt;P&gt;1. SILICON &amp;amp; FIRMWARE COMPATIBILITY&lt;BR /&gt;- Will identical firmware binary (we developed ourselves) run identically on Malaysia-sourced S32K312HVS without recompilation?&lt;BR /&gt;- Are there ANY silicon-level differences between China and Malaysia MCUs (same part number)?&lt;/P&gt;&lt;P&gt;2. SPECIFICATION CONSISTENCY&lt;BR /&gt;– exact match on Malaysia MCUs?&lt;BR /&gt;- Reset module (RGM: FREC/FRET/DREC/DRET counters) – identical behavior?&lt;BR /&gt;- FlexCAN peripheral (500 kbps, ISO-TP) – no variations?&lt;BR /&gt;- Clock accuracy &amp;amp; PLL lock time – same specs?&lt;/P&gt;&lt;P&gt;3. ERRATA &amp;amp; WORKAROUNDS&lt;BR /&gt;- Current firmware includes workarounds (RGM escalation, CAN timeout handling).&lt;BR /&gt;- Are these workarounds still valid on Malaysia MCUs, or do we need adjustments?&lt;BR /&gt;- Any NEW errata specific to Malaysia production?&lt;/P&gt;&lt;P&gt;4. PROCESS VARIATIONS&lt;BR /&gt;- Any electrical parameter shifts (timing, power, temperature coefficient)?&lt;BR /&gt;- ECC reliability differences on Malaysia-sourced Flash/NVM?&lt;/P&gt;&lt;P&gt;Please confirm: Can we use the SAME firmware binary and expect IDENTICAL product&lt;BR /&gt;behavior on Malaysia MCUs, or are adjustments required?&lt;/P&gt;&lt;P&gt;Timeline: Phase 1 validation starts in the end of September. Your quick response would be appreciated.&lt;/P&gt;</description>
    <pubDate>Thu, 03 Sep 2026 00:57:05 GMT</pubDate>
    <dc:creator>DWYUN</dc:creator>
    <dc:date>2026-09-03T00:57:05Z</dc:date>
    <item>
      <title>S32K312 Firmware-Compatibility</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-Firmware-Compatibility/m-p/2410720#M60850</link>
      <description>&lt;P&gt;Hello NXP Support,&lt;/P&gt;&lt;P&gt;We are developing TPMS controllers using S32K312HVS MCUs.&lt;BR /&gt;Currently sourced from China (Rev: 0P09C), we are transitioning to Malaysia production (same MCU model).&lt;/P&gt;&lt;P&gt;For Phase 1 validation, please confirm the following:&lt;/P&gt;&lt;P&gt;1. SILICON &amp;amp; FIRMWARE COMPATIBILITY&lt;BR /&gt;- Will identical firmware binary (we developed ourselves) run identically on Malaysia-sourced S32K312HVS without recompilation?&lt;BR /&gt;- Are there ANY silicon-level differences between China and Malaysia MCUs (same part number)?&lt;/P&gt;&lt;P&gt;2. SPECIFICATION CONSISTENCY&lt;BR /&gt;– exact match on Malaysia MCUs?&lt;BR /&gt;- Reset module (RGM: FREC/FRET/DREC/DRET counters) – identical behavior?&lt;BR /&gt;- FlexCAN peripheral (500 kbps, ISO-TP) – no variations?&lt;BR /&gt;- Clock accuracy &amp;amp; PLL lock time – same specs?&lt;/P&gt;&lt;P&gt;3. ERRATA &amp;amp; WORKAROUNDS&lt;BR /&gt;- Current firmware includes workarounds (RGM escalation, CAN timeout handling).&lt;BR /&gt;- Are these workarounds still valid on Malaysia MCUs, or do we need adjustments?&lt;BR /&gt;- Any NEW errata specific to Malaysia production?&lt;/P&gt;&lt;P&gt;4. PROCESS VARIATIONS&lt;BR /&gt;- Any electrical parameter shifts (timing, power, temperature coefficient)?&lt;BR /&gt;- ECC reliability differences on Malaysia-sourced Flash/NVM?&lt;/P&gt;&lt;P&gt;Please confirm: Can we use the SAME firmware binary and expect IDENTICAL product&lt;BR /&gt;behavior on Malaysia MCUs, or are adjustments required?&lt;/P&gt;&lt;P&gt;Timeline: Phase 1 validation starts in the end of September. Your quick response would be appreciated.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Sep 2026 00:57:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-Firmware-Compatibility/m-p/2410720#M60850</guid>
      <dc:creator>DWYUN</dc:creator>
      <dc:date>2026-09-03T00:57:05Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 Firmware-Compatibility</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-Firmware-Compatibility/m-p/2410843#M60862</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The S32K3xx ordering part number system uses a "N" prefix to designate "Non-China manufacturing qualified ordering part number." &lt;A id="base-ui-:r6q:" tabindex="0" role="button" href="https://www.nxp.com/docs/en/data-sheet/S32K3xx.pdf" rel="noreferrer" aria-expanded="false" aria-haspopup="dialog" data-base-ui-click-trigger="" data-label="2" aria-label="Citation 2" target="_blank"&gt;&lt;/A&gt;This is purely a sourcing/ordering designation. Critically, it does not indicate a new mask set or silicon revision — the same die/mask (0P09C) is used. The Malaysia assembly/test site is ATKL (Petaling Jaya, Malaysia), which is NXP's qualified assembly and test facility for the S32K family.&lt;/P&gt;
&lt;P&gt;What you have to pay attention is the mask revision&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_0-1788419667576.png" style="width: 601px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395824iC6CBA7DB0DD5CE77/image-dimensions/601x347?v=v2" width="601" height="347" role="button" title="petervlna_0-1788419667576.png" alt="petervlna_0-1788419667576.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;petervlna_0-1788419667576.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_1-1788419699369.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395825iF324D7197BFB5CE5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="petervlna_1-1788419699369.png" alt="petervlna_1-1788419699369.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;petervlna_1-1788419699369.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The "N" prefix is essentially a supply chain resilience and geopolitical risk mitigation tool. It gives customers:&lt;/P&gt;
&lt;P&gt;Guaranteed non-China assembly &amp;amp; test — the device is assembled and tested exclusively at non-China sites (e.g., ATKL Petaling Jaya, Malaysia). Customers who have contractual, regulatory, or policy requirements to avoid China-origin manufacturing can source the "N" variant to satisfy those requirements.&lt;/P&gt;
&lt;P&gt;Export control / trade compliance — some customers (especially in defense-adjacent, government, or regulated automotive supply chains) are required to document and control country-of-origin for components. The "N" variant provides a clean audit trail.&lt;/P&gt;
&lt;P&gt;Supply diversification — having both "S" and "N" qualified variants gives customers flexibility to switch sourcing without re-qualification, since both variants share the same silicon die, mask set, and electrical specifications.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Thu, 03 Sep 2026 07:18:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-Firmware-Compatibility/m-p/2410843#M60862</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2026-09-03T07:18:20Z</dc:date>
    </item>
  </channel>
</rss>