<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 PDB pulse-out trigger ADC in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-PDB-pulse-out-trigger-ADC/m-p/2410337#M60829</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;DIV&gt;
&lt;P&gt;It is possible to trigger the ADC from a PDB Pulse-Out signal, and the trigger muxing table shows this connection as a valid option.&lt;/P&gt;
&lt;P&gt;However, the default hardware triggering scheme uses the PDB to trigger the ADC directly, which is the recommended approach. In this mode, the PDB generates all required channel pre-triggers as well as the ADC hardware trigger.&lt;/P&gt;
&lt;P&gt;An alternative hardware triggering scheme is to use TRGMUX, selected by SIM_ADCOPT[ADCxTRGSEL].&lt;/P&gt;
&lt;P&gt;A drawback of this approach is the limited number of pre-triggers (four) and their hardware availability. Only LPIT supports hardware pre-triggers. For other trigger sources, software pre-triggers must be configured using SIM_ADCOPT[ADCxSWPRETRG].&lt;/P&gt;
&lt;P&gt;Therefore, in your case, you would need to configure the software pre-trigger before each PDB Pulse-Out event that is used as the ADC hardware trigger.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;
&lt;/DIV&gt;</description>
    <pubDate>Wed, 02 Sep 2026 07:07:13 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2026-09-02T07:07:13Z</dc:date>
    <item>
      <title>S32K144 PDB pulse-out trigger ADC</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-PDB-pulse-out-trigger-ADC/m-p/2410261#M60823</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="joshua9264_0-1788314383945.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395725iF660D7C876C9D7E1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="joshua9264_0-1788314383945.png" alt="joshua9264_0-1788314383945.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;joshua9264_0-1788314383945.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="joshua9264_1-1788314500502.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395726i0475E887374BC398/image-size/medium?v=v2&amp;amp;px=400" role="button" title="joshua9264_1-1788314500502.png" alt="joshua9264_1-1788314500502.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;joshua9264_1-1788314500502.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;#S32K144，Can I use Pulse-OUT to trigger ADC conversion？&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2026 02:05:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-PDB-pulse-out-trigger-ADC/m-p/2410261#M60823</guid>
      <dc:creator>joshua9264</dc:creator>
      <dc:date>2026-09-02T02:05:20Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 PDB pulse-out trigger ADC</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-PDB-pulse-out-trigger-ADC/m-p/2410337#M60829</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;DIV&gt;
&lt;P&gt;It is possible to trigger the ADC from a PDB Pulse-Out signal, and the trigger muxing table shows this connection as a valid option.&lt;/P&gt;
&lt;P&gt;However, the default hardware triggering scheme uses the PDB to trigger the ADC directly, which is the recommended approach. In this mode, the PDB generates all required channel pre-triggers as well as the ADC hardware trigger.&lt;/P&gt;
&lt;P&gt;An alternative hardware triggering scheme is to use TRGMUX, selected by SIM_ADCOPT[ADCxTRGSEL].&lt;/P&gt;
&lt;P&gt;A drawback of this approach is the limited number of pre-triggers (four) and their hardware availability. Only LPIT supports hardware pre-triggers. For other trigger sources, software pre-triggers must be configured using SIM_ADCOPT[ADCxSWPRETRG].&lt;/P&gt;
&lt;P&gt;Therefore, in your case, you would need to configure the software pre-trigger before each PDB Pulse-Out event that is used as the ADC hardware trigger.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Wed, 02 Sep 2026 07:07:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-PDB-pulse-out-trigger-ADC/m-p/2410337#M60829</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2026-09-02T07:07:13Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 PDB pulse-out trigger ADC</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-PDB-pulse-out-trigger-ADC/m-p/2410359#M60830</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="joshua9264_1-1788335844473.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395754i3D1F107AD4B33C92/image-size/medium?v=v2&amp;amp;px=400" role="button" title="joshua9264_1-1788335844473.png" alt="joshua9264_1-1788335844473.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;joshua9264_1-1788335844473.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This config is&amp;nbsp;valid，thank you&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2026 08:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-PDB-pulse-out-trigger-ADC/m-p/2410359#M60830</guid>
      <dc:creator>joshua9264</dc:creator>
      <dc:date>2026-09-02T08:03:08Z</dc:date>
    </item>
  </channel>
</rss>