<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic eMcem_Fcc_Init failed to clear errors in S32K</title>
    <link>https://community.nxp.com/t5/S32K/eMcem-Fcc-Init-failed-to-clear-errors/m-p/2408548#M60703</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I run the application on S32K388 and then attach trace32 debugger.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In eMcem_Fcc_Init(), read NCF_S0 status register returns u32ReadBack&lt;STRONG&gt;=0x5&lt;/STRONG&gt; (&lt;STRONG&gt;NCF[0]&lt;/STRONG&gt;&amp;nbsp;HSE lockstep error and &lt;STRONG&gt;NCF[2]&lt;/STRONG&gt; ECC error).&amp;nbsp;&lt;/P&gt;&lt;P&gt;and eMcem_Fccu_ClearFault()&amp;nbsp;doesn't clear the faults too.&lt;/P&gt;&lt;P&gt;How can I clear the faults to make eMcem_Fcc_Init() and eMcem_Init() initialised successfully?&amp;nbsp; What could be the issue ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sara&lt;/P&gt;</description>
    <pubDate>Wed, 26 Aug 2026 14:38:18 GMT</pubDate>
    <dc:creator>Sara_Sara</dc:creator>
    <dc:date>2026-08-26T14:38:18Z</dc:date>
    <item>
      <title>eMcem_Fcc_Init failed to clear errors</title>
      <link>https://community.nxp.com/t5/S32K/eMcem-Fcc-Init-failed-to-clear-errors/m-p/2408548#M60703</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I run the application on S32K388 and then attach trace32 debugger.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In eMcem_Fcc_Init(), read NCF_S0 status register returns u32ReadBack&lt;STRONG&gt;=0x5&lt;/STRONG&gt; (&lt;STRONG&gt;NCF[0]&lt;/STRONG&gt;&amp;nbsp;HSE lockstep error and &lt;STRONG&gt;NCF[2]&lt;/STRONG&gt; ECC error).&amp;nbsp;&lt;/P&gt;&lt;P&gt;and eMcem_Fccu_ClearFault()&amp;nbsp;doesn't clear the faults too.&lt;/P&gt;&lt;P&gt;How can I clear the faults to make eMcem_Fcc_Init() and eMcem_Init() initialised successfully?&amp;nbsp; What could be the issue ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sara&lt;/P&gt;</description>
      <pubDate>Wed, 26 Aug 2026 14:38:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/eMcem-Fcc-Init-failed-to-clear-errors/m-p/2408548#M60703</guid>
      <dc:creator>Sara_Sara</dc:creator>
      <dc:date>2026-08-26T14:38:18Z</dc:date>
    </item>
    <item>
      <title>Re: eMcem_Fcc_Init failed to clear errors</title>
      <link>https://community.nxp.com/t5/S32K/eMcem-Fcc-Init-failed-to-clear-errors/m-p/2408757#M60715</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;NCF_S0 = 0x5 indicates that both FCCU NCF[0] (lockstep/core fault) and NCF[2] (ECC fault) are active. On S32K3 devices, these fault flags are retained after an FCCU functional reset so that software can identify the root cause. The FCCU fault status cannot be cleared while the originating error condition is still present. Therefore, the issue is likely not in eMcem_Fccu_ClearFault(), but that a lockstep fault and an ECC fault are still being reported by the underlying hardware.&lt;/P&gt;
&lt;P&gt;Please check the corresponding FCCU, RCCU/DCMROD, and ERM status registers to identify the exact source. Since the issue occurs after attaching TRACE32, also verify that FCCU Debug Mode is enabled and compare behavior when the debugger is connected from reset.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Thu, 27 Aug 2026 09:00:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/eMcem-Fcc-Init-failed-to-clear-errors/m-p/2408757#M60715</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2026-08-27T09:00:15Z</dc:date>
    </item>
  </channel>
</rss>