<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K358 Not Receiving UART RX Data in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K358-Not-Receiving-UART-RX-Data/m-p/2408170#M60658</link>
    <description>&lt;P&gt;I am trying to test uart communication on FRDM A S32K358 board. Used the UART6 tx and rx in this in trasmission i can see data on tera term as expected also on debugger seeing&amp;nbsp;Lpuart_Uart_Ip_SyncSend api status is successful. But when i am trying to do for&amp;nbsp; receiver uart6rx pin it&amp;nbsp;Lpuart_Uart_Ip_SyncReceive(UART_LPUART_INTERNAL_CHANNEL, rxData, 1, 10000) got response timeout.&amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;So i checked with different uart like Uart3 in that case also same behaviour then i tried to configure PTD3 &amp;amp; PTD2 acts as gpio and try to set both pin in that case PTD3 is not set (not change any behavior) but PTD2 set to 1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please suggest how i can check rx data i am trying to do hardware loopback on pin. as i am dont have logic analyzer.&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ankita_0-1787651884647.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395302iC99234D98C93AD62/image-size/medium?v=v2&amp;amp;px=400" alt="Ankita_0-1787651884647.png" title="Ankita_0-1787651884647.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 25 Aug 2026 09:58:13 GMT</pubDate>
    <dc:creator>Ankita</dc:creator>
    <dc:date>2026-08-25T09:58:13Z</dc:date>
    <item>
      <title>S32K358 Not Receiving UART RX Data</title>
      <link>https://community.nxp.com/t5/S32K/S32K358-Not-Receiving-UART-RX-Data/m-p/2408170#M60658</link>
      <description>&lt;P&gt;I am trying to test uart communication on FRDM A S32K358 board. Used the UART6 tx and rx in this in trasmission i can see data on tera term as expected also on debugger seeing&amp;nbsp;Lpuart_Uart_Ip_SyncSend api status is successful. But when i am trying to do for&amp;nbsp; receiver uart6rx pin it&amp;nbsp;Lpuart_Uart_Ip_SyncReceive(UART_LPUART_INTERNAL_CHANNEL, rxData, 1, 10000) got response timeout.&amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;So i checked with different uart like Uart3 in that case also same behaviour then i tried to configure PTD3 &amp;amp; PTD2 acts as gpio and try to set both pin in that case PTD3 is not set (not change any behavior) but PTD2 set to 1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please suggest how i can check rx data i am trying to do hardware loopback on pin. as i am dont have logic analyzer.&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ankita_0-1787651884647.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395302iC99234D98C93AD62/image-size/medium?v=v2&amp;amp;px=400" alt="Ankita_0-1787651884647.png" title="Ankita_0-1787651884647.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Aug 2026 09:58:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K358-Not-Receiving-UART-RX-Data/m-p/2408170#M60658</guid>
      <dc:creator>Ankita</dc:creator>
      <dc:date>2026-08-25T09:58:13Z</dc:date>
    </item>
  </channel>
</rss>