<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K312MINI-EVB in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312MINI-EVB/m-p/2408049#M60652</link>
    <description>&lt;P class=""&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using an &lt;STRONG&gt;NXP S32K312MINI-EVB&lt;/STRONG&gt; board.&lt;/P&gt;&lt;P&gt;Initially, the board was powered ON and the LEDs were working, but the USB connection was not detected by Windows Device Manager.&lt;/P&gt;&lt;P&gt;I verified that the PEmicro driver is installed. Device Manager shows:&lt;/P&gt;&lt;P&gt;Jungo Connectivity → pemicrovincdrv&lt;/P&gt;&lt;P&gt;I also tested the board with another PC and another USB connection, but the board was not detected.&lt;/P&gt;&lt;P&gt;During troubleshooting, while the board was connected through USB, I removed the &lt;STRONG&gt;J19 and J20 jumpers&lt;/STRONG&gt;. The board LEDs turned OFF.&lt;/P&gt;&lt;P&gt;I then put the jumpers back, but now the board does not power on when i tried to give power supply though USB . when I supply &lt;STRONG&gt;12 V through J1 only RGB led is ON.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;According to the S32K312MINI-EVB Hardware User Manual:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;USB-C J9 → J19 = 1–2, J20 = 1–2&lt;/LI&gt;&lt;LI&gt;12 V J1 → J19 = 2–3, J20 = 2–3&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I have set J19/J20 accordingly, but the power LED remains OFF.&lt;/P&gt;&lt;P&gt;Could someone please help me determine whether the board's power circuit may have been affected and which test points I should measure?&lt;/P&gt;&lt;P&gt;I can provide photos of the board and voltage measurements at J23 (VBAT), J24 (VBST), J16 (P5V0), J17 (P3V3), and J27 (GND).&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Tue, 25 Aug 2026 06:44:09 GMT</pubDate>
    <dc:creator>NagarajBahaddur</dc:creator>
    <dc:date>2026-08-25T06:44:09Z</dc:date>
    <item>
      <title>S32K312MINI-EVB</title>
      <link>https://community.nxp.com/t5/S32K/S32K312MINI-EVB/m-p/2408049#M60652</link>
      <description>&lt;P class=""&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using an &lt;STRONG&gt;NXP S32K312MINI-EVB&lt;/STRONG&gt; board.&lt;/P&gt;&lt;P&gt;Initially, the board was powered ON and the LEDs were working, but the USB connection was not detected by Windows Device Manager.&lt;/P&gt;&lt;P&gt;I verified that the PEmicro driver is installed. Device Manager shows:&lt;/P&gt;&lt;P&gt;Jungo Connectivity → pemicrovincdrv&lt;/P&gt;&lt;P&gt;I also tested the board with another PC and another USB connection, but the board was not detected.&lt;/P&gt;&lt;P&gt;During troubleshooting, while the board was connected through USB, I removed the &lt;STRONG&gt;J19 and J20 jumpers&lt;/STRONG&gt;. The board LEDs turned OFF.&lt;/P&gt;&lt;P&gt;I then put the jumpers back, but now the board does not power on when i tried to give power supply though USB . when I supply &lt;STRONG&gt;12 V through J1 only RGB led is ON.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;According to the S32K312MINI-EVB Hardware User Manual:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;USB-C J9 → J19 = 1–2, J20 = 1–2&lt;/LI&gt;&lt;LI&gt;12 V J1 → J19 = 2–3, J20 = 2–3&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I have set J19/J20 accordingly, but the power LED remains OFF.&lt;/P&gt;&lt;P&gt;Could someone please help me determine whether the board's power circuit may have been affected and which test points I should measure?&lt;/P&gt;&lt;P&gt;I can provide photos of the board and voltage measurements at J23 (VBAT), J24 (VBST), J16 (P5V0), J17 (P3V3), and J27 (GND).&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 25 Aug 2026 06:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312MINI-EVB/m-p/2408049#M60652</guid>
      <dc:creator>NagarajBahaddur</dc:creator>
      <dc:date>2026-08-25T06:44:09Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312MINI-EVB</title>
      <link>https://community.nxp.com/t5/S32K/S32K312MINI-EVB/m-p/2408420#M60695</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please do not use a USB hub; connect the USB cable directly to the computer. I recommend connecting via USB 3.0 or Type-C port.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="S32K312MINI on board debugger.png" style="width: 663px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395358i2F3117A4E09FD040/image-size/large?v=v2&amp;amp;px=999" role="button" title="S32K312MINI on board debugger.png" alt="S32K312MINI on board debugger.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;S32K312MINI on board debugger.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Does the red OSDA_LED D9 light up?&lt;/P&gt;
&lt;P&gt;Otherwise, OpenSDA may not work properly, which would prevent the onboard debugger from being used.&lt;/P&gt;
&lt;P&gt;Please check the voltage one by one according to the schematic diagram.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
      <pubDate>Wed, 26 Aug 2026 09:14:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312MINI-EVB/m-p/2408420#M60695</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2026-08-26T09:14:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312MINI-EVB</title>
      <link>https://community.nxp.com/t5/S32K/S32K312MINI-EVB/m-p/2409461#M60751</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;When powered by USB (J19 1-2, J20 1-2), pin 2 of J19 measures 12V, and pin 2 of J20 measures 5V. The red OSDA_LED on D9 is lit.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="UM12505 Table 3. Supply board method (low current).png" style="width: 994px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395554iFF68ABCEA6F915F4/image-size/large?v=v2&amp;amp;px=999" role="button" title="UM12505 Table 3. Supply board method (low current).png" alt="UM12505 Table 3. Supply board method (low current).png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;UM12505 Table 3. Supply board method (low current).png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;When powered externally by J1 (J19 2-3, J20 2-3), pin 2 of both J19 and J20 measures 12V. No LED is lit. In this case, an external debugger needs to be connected to J7 to download programs to the S32K312.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="UM12505 Table 4. Supply board method (high current).png" style="width: 989px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395555i679274002CFA5EB3/image-size/large?v=v2&amp;amp;px=999" role="button" title="UM12505 Table 4. Supply board method (high current).png" alt="UM12505 Table 4. Supply board method (high current).png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;UM12505 Table 4. Supply board method (high current).png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Also, please refer to &lt;STRONG&gt;Figure 3. Main THP for power measurements&lt;/STRONG&gt; in &lt;A href="https://www.nxp.com/webapp/Download?colCode=UM12505" target="_self"&gt;UM12505, FRDM-A-S32K312 development board for MCUs hardware user manual&lt;/A&gt; to check if it conforms to &lt;STRONG&gt;Table 5. Through hole pads for measure voltages&lt;/STRONG&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="UM12505 Table 5. Through hole pads for measure voltages Figure 3. Main THP for power measurements.png" style="width: 984px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395556iBDAADD5BBCCA5F17/image-size/large?v=v2&amp;amp;px=999" role="button" title="UM12505 Table 5. Through hole pads for measure voltages Figure 3. Main THP for power measurements.png" alt="UM12505 Table 5. Through hole pads for measure voltages Figure 3. Main THP for power measurements.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;UM12505 Table 5. Through hole pads for measure voltages Figure 3. Main THP for power measurements.png&lt;/span&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 31 Aug 2026 02:47:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312MINI-EVB/m-p/2409461#M60751</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2026-08-31T02:47:43Z</dc:date>
    </item>
  </channel>
</rss>