<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K312 LPSPI Slave mode in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-LPSPI-Slave-mode/m-p/2407225#M60601</link>
    <description>OK，thank you</description>
    <pubDate>Fri, 21 Aug 2026 07:10:56 GMT</pubDate>
    <dc:creator>joshua9264</dc:creator>
    <dc:date>2026-08-21T07:10:56Z</dc:date>
    <item>
      <title>S32K312 LPSPI Slave mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-LPSPI-Slave-mode/m-p/2406529#M60560</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="joshua9264_0-1787132569429.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394950i93F6D7C23A6ED221/image-size/medium?v=v2&amp;amp;px=400" role="button" title="joshua9264_0-1787132569429.png" alt="joshua9264_0-1787132569429.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;working：slave mode、4 lines&lt;/P&gt;&lt;P&gt;(B) is right or (C) is right？&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Aug 2026 09:47:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-LPSPI-Slave-mode/m-p/2406529#M60560</guid>
      <dc:creator>joshua9264</dc:creator>
      <dc:date>2026-08-19T09:47:13Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 LPSPI Slave mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-LPSPI-Slave-mode/m-p/2406707#M60569</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262511"&gt;@joshua9264&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Both configurations are valid.&lt;/P&gt;
&lt;P&gt;By default, the LPSPI interface operates according to Option B, where:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;SIN as the input data line, connected to the master's output.&lt;/LI&gt;
&lt;LI&gt;SOUT as the output data line, connected to the master's input.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;However, it is also possible to swap the data pin directions so that SOUT is used as the input data line and SIN is used as the output data line, which corresponds to Option C. To achieve this configuration, you need to set the CFGR1[PINCFG] field accordingly.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Wed, 19 Aug 2026 20:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-LPSPI-Slave-mode/m-p/2406707#M60569</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2026-08-19T20:26:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 LPSPI Slave mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-LPSPI-Slave-mode/m-p/2407225#M60601</link>
      <description>OK，thank you</description>
      <pubDate>Fri, 21 Aug 2026 07:10:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-LPSPI-Slave-mode/m-p/2407225#M60601</guid>
      <dc:creator>joshua9264</dc:creator>
      <dc:date>2026-08-21T07:10:56Z</dc:date>
    </item>
  </channel>
</rss>