<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: About S32K3XX APPLICATION in S32K</title>
    <link>https://community.nxp.com/t5/S32K/About-S32K3XX-APPLICATION/m-p/2406195#M60542</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;I'd like to ask why there's no `Cache_Ip_init()` function in the S32K358 RTD library. If there's no initialization function, how does the system initialize the cache? Does the system automatically start the cache initialization process?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;The S32K358 RTD does not provide a dedicated Cache_Ip_Init() API in recent RTD releases. Cache enablement is handled during device startup through platform/system initialization code. After the cache is enabled, the Cortex-M7 hardware automatically manages cache allocation, invalidation, and line replacement. Therefore, no explicit application-level cache initialization function is required.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
    <pubDate>Tue, 18 Aug 2026 11:36:15 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2026-08-18T11:36:15Z</dc:date>
    <item>
      <title>About S32K3XX APPLICATION</title>
      <link>https://community.nxp.com/t5/S32K/About-S32K3XX-APPLICATION/m-p/2406149#M60539</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sunshine88_0-1787046454804.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394851iC977B9E5E86CF6C9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sunshine88_0-1787046454804.png" alt="sunshine88_0-1787046454804.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;sunshine88_0-1787046454804.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;想咨询一下，为什么在S32K358 RTD库函数中，没有Cache_Ip_init()函数，如果没有初始化函数，系统又是怎样初始的哪？系统自启动Cache初始化过程吗？&lt;/P&gt;</description>
      <pubDate>Tue, 18 Aug 2026 09:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-S32K3XX-APPLICATION/m-p/2406149#M60539</guid>
      <dc:creator>sunshine88</dc:creator>
      <dc:date>2026-08-18T09:49:55Z</dc:date>
    </item>
    <item>
      <title>Re: About S32K3XX APPLICATION</title>
      <link>https://community.nxp.com/t5/S32K/About-S32K3XX-APPLICATION/m-p/2406195#M60542</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;I'd like to ask why there's no `Cache_Ip_init()` function in the S32K358 RTD library. If there's no initialization function, how does the system initialize the cache? Does the system automatically start the cache initialization process?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;The S32K358 RTD does not provide a dedicated Cache_Ip_Init() API in recent RTD releases. Cache enablement is handled during device startup through platform/system initialization code. After the cache is enabled, the Cortex-M7 hardware automatically manages cache allocation, invalidation, and line replacement. Therefore, no explicit application-level cache initialization function is required.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Tue, 18 Aug 2026 11:36:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-S32K3XX-APPLICATION/m-p/2406195#M60542</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2026-08-18T11:36:15Z</dc:date>
    </item>
  </channel>
</rss>