<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K358 LPSPI0 and LPSPI2 not work</title>
    <link>https://community.nxp.com/t5/S32K/S32K358-LPSPI0-and-LPSPI2-not-work/m-p/2405659#M60498</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;DIV&gt;
&lt;P&gt;Please double-check the SpiHwUnit assignment for each SpiExternalDevice.&lt;/P&gt;
&lt;P&gt;From the screenshots, SpiExternalDevice_2 appears to be assigned to CSIB0, while the SpiPhyUnit configuration shows multiple SPI hardware units. If SpiExternalDevice_2 is intended to communicate through a different LPSPI instance, its SpiHwUnit reference must point to the corresponding SPI hardware unit configured for that instance.&lt;/P&gt;
&lt;P&gt;The mapping between SpiExternalDevice_x and SpiPhyUnit entries is user-configurable, so the numbering does not necessarily need to match. However, the SpiHwUnit assignment must be consistent with the LPSPI instance that is intended to perform the transfer.&lt;/P&gt;
&lt;P&gt;From the screenshots, SpiExternalDevice_2 seems to be configured to use CSIB0, which corresponds to the first SPI hardware unit defined in SpiPhyUnit, but its setting is not seen.&lt;BR /&gt;Besides 3rd hardware unit is configured for LPSPI_2. If the intention is to communicate through LPSPI_2, then SpiExternalDevice_2 should reference the SpiPhyUnit associated with that LPSPI instance (CSIB2) rather than CSIB0.&lt;/P&gt;
&lt;P&gt;Please verify that each SpiExternalDevice references the correct SpiPhyUnit (CSIBx) associated with the desired LPSPI peripheral. An incorrect assignment could explain why transfers are observed only on one SPI instance.&lt;BR /&gt;&lt;BR /&gt;BR, Petr&lt;/P&gt;
&lt;/DIV&gt;</description>
    <pubDate>Mon, 17 Aug 2026 07:08:56 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2026-08-17T07:08:56Z</dc:date>
    <item>
      <title>S32K358 LPSPI0 and LPSPI2 not work</title>
      <link>https://community.nxp.com/t5/S32K/S32K358-LPSPI0-and-LPSPI2-not-work/m-p/2405506#M60490</link>
      <description>&lt;P&gt;Hello NXP helper.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;RTD:7.0.1&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Licunhao_5-1786787375079.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394691iF964218D8F99F31F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Licunhao_5-1786787375079.png" alt="Licunhao_5-1786787375079.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;S32DS3.6.10&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Licunhao_3-1786787331998.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394689i954D4A7303014379/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Licunhao_3-1786787331998.png" alt="Licunhao_3-1786787331998.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Licunhao_4-1786787354386.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394690i3E7A49617D91388B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Licunhao_4-1786787354386.png" alt="Licunhao_4-1786787354386.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use S32K358 LPSPI0 LPSPI1 LPSPI2 Only LPSPI1 can work, LPSPI0 and LPSPI2 not work. I found some pin configs different.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Licunhao_0-1786787130994.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394686i047C6D6D39ECFC2C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Licunhao_0-1786787130994.png" alt="Licunhao_0-1786787130994.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Licunhao_1-1786787179244.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394687i954F8215DFC78F64/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Licunhao_1-1786787179244.png" alt="Licunhao_1-1786787179244.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Three LPSPI use for Master.And I use Sync transmit API.RTD 7.0.1&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Licunhao_2-1786787237518.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394688i5AB9B7E5236A5C93/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Licunhao_2-1786787237518.png" alt="Licunhao_2-1786787237518.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But I can only get LPSPI1 output.&lt;/P&gt;&lt;P&gt;Is there any config I need do?&lt;/P&gt;&lt;P&gt;Please give me a help.&lt;/P&gt;</description>
      <pubDate>Sat, 15 Aug 2026 09:49:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K358-LPSPI0-and-LPSPI2-not-work/m-p/2405506#M60490</guid>
      <dc:creator>Licunhao</dc:creator>
      <dc:date>2026-08-15T09:49:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32K358 LPSPI0 and LPSPI2 not work</title>
      <link>https://community.nxp.com/t5/S32K/S32K358-LPSPI0-and-LPSPI2-not-work/m-p/2405659#M60498</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;DIV&gt;
&lt;P&gt;Please double-check the SpiHwUnit assignment for each SpiExternalDevice.&lt;/P&gt;
&lt;P&gt;From the screenshots, SpiExternalDevice_2 appears to be assigned to CSIB0, while the SpiPhyUnit configuration shows multiple SPI hardware units. If SpiExternalDevice_2 is intended to communicate through a different LPSPI instance, its SpiHwUnit reference must point to the corresponding SPI hardware unit configured for that instance.&lt;/P&gt;
&lt;P&gt;The mapping between SpiExternalDevice_x and SpiPhyUnit entries is user-configurable, so the numbering does not necessarily need to match. However, the SpiHwUnit assignment must be consistent with the LPSPI instance that is intended to perform the transfer.&lt;/P&gt;
&lt;P&gt;From the screenshots, SpiExternalDevice_2 seems to be configured to use CSIB0, which corresponds to the first SPI hardware unit defined in SpiPhyUnit, but its setting is not seen.&lt;BR /&gt;Besides 3rd hardware unit is configured for LPSPI_2. If the intention is to communicate through LPSPI_2, then SpiExternalDevice_2 should reference the SpiPhyUnit associated with that LPSPI instance (CSIB2) rather than CSIB0.&lt;/P&gt;
&lt;P&gt;Please verify that each SpiExternalDevice references the correct SpiPhyUnit (CSIBx) associated with the desired LPSPI peripheral. An incorrect assignment could explain why transfers are observed only on one SPI instance.&lt;BR /&gt;&lt;BR /&gt;BR, Petr&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Mon, 17 Aug 2026 07:08:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K358-LPSPI0-and-LPSPI2-not-work/m-p/2405659#M60498</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2026-08-17T07:08:56Z</dc:date>
    </item>
  </channel>
</rss>