<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: NXP S32K312 CAN0 – FIRC vs. FXOSC Clock Source Causing CAN Errors</title>
    <link>https://community.nxp.com/t5/S32K/NXP-S32K312-CAN0-FIRC-vs-FXOSC-Clock-Source-Causing-CAN-Errors/m-p/2404657#M60468</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/255495"&gt;@Karthik_R&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Usually, FIRC clock is not recommended for FlexCAN communication, as accuracy is over the ~1% requirement according to&amp;nbsp;CAN protocol (ISO 11898-1). You can see from S32K3's Data Sheet that FIRC's deviation is +- 5%.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Recommendation is to use either FXOSC or PLL running from XOSC. You can refer to&amp;nbsp;&lt;A href="https://www.google.com/url?sa=t&amp;amp;rct=j&amp;amp;q=&amp;amp;esrc=s&amp;amp;source=web&amp;amp;cd=&amp;amp;ved=2ahUKEwiC_IW5mJ6WAxXXlmoFHWR1LTAQFnoECB0QAQ&amp;amp;url=https%3A%2F%2Fcommunity.nxp.com%2Fpwmxy87654%2Fattachments%2Fpwmxy87654%2Fmpc5xxx%2540tkb%2F292%2F1%2FFlexCAN%2520bit%2520timing.pdf&amp;amp;usg=AOvVaw0709bky-w7TbDa1ql2Tz2v&amp;amp;opi=89978449" target="_blank"&gt;FlexCAN Bit Timing Calculation&lt;/A&gt;&amp;nbsp;document, and&amp;nbsp;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5xxx-S32Kxx-LPCxxxx-CAN-CAN-FD-bit-timing-calculation/ta-p/1119319" target="_blank"&gt;MPC5xxx/S32Kxx/LPCxxxx: CAN / CAN FD bit timing calculation&lt;/A&gt;&amp;nbsp;tool for clock and timing calculations.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Hope this is clear.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 13 Aug 2026 18:14:29 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2026-08-13T18:14:29Z</dc:date>
    <item>
      <title>NXP S32K312 CAN0 – FIRC vs. FXOSC Clock Source Causing CAN Errors</title>
      <link>https://community.nxp.com/t5/S32K/NXP-S32K312-CAN0-FIRC-vs-FXOSC-Clock-Source-Causing-CAN-Errors/m-p/2404460#M60460</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I am using CAN0 on the S32K312 at 500 kbps with an 87.5% sampling point.&lt;/P&gt;&lt;P&gt;Initially, I set up CAN0 to use the internal FIRC_CLK as the clock source. When I connected the S32K312 to a network with multiple CAN nodes, I noticed a lot of CAN error frames.&lt;/P&gt;&lt;P&gt;I then switched the CAN clock source from FIRC_CLK to the external FXOSC_CLK while keeping the CAN bitrate and sampling point the same. After this change, the communication became stable, and I stopped seeing the error frames.&lt;/P&gt;&lt;P&gt;Could anyone help me understand why switching the clock source from FIRC_CLK to FXOSC_CLK would fix the CAN errors?&lt;/P&gt;</description>
      <pubDate>Thu, 13 Aug 2026 08:11:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NXP-S32K312-CAN0-FIRC-vs-FXOSC-Clock-Source-Causing-CAN-Errors/m-p/2404460#M60460</guid>
      <dc:creator>Karthik_R</dc:creator>
      <dc:date>2026-08-13T08:11:49Z</dc:date>
    </item>
    <item>
      <title>Re: NXP S32K312 CAN0 – FIRC vs. FXOSC Clock Source Causing CAN Errors</title>
      <link>https://community.nxp.com/t5/S32K/NXP-S32K312-CAN0-FIRC-vs-FXOSC-Clock-Source-Causing-CAN-Errors/m-p/2404657#M60468</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/255495"&gt;@Karthik_R&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Usually, FIRC clock is not recommended for FlexCAN communication, as accuracy is over the ~1% requirement according to&amp;nbsp;CAN protocol (ISO 11898-1). You can see from S32K3's Data Sheet that FIRC's deviation is +- 5%.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Recommendation is to use either FXOSC or PLL running from XOSC. You can refer to&amp;nbsp;&lt;A href="https://www.google.com/url?sa=t&amp;amp;rct=j&amp;amp;q=&amp;amp;esrc=s&amp;amp;source=web&amp;amp;cd=&amp;amp;ved=2ahUKEwiC_IW5mJ6WAxXXlmoFHWR1LTAQFnoECB0QAQ&amp;amp;url=https%3A%2F%2Fcommunity.nxp.com%2Fpwmxy87654%2Fattachments%2Fpwmxy87654%2Fmpc5xxx%2540tkb%2F292%2F1%2FFlexCAN%2520bit%2520timing.pdf&amp;amp;usg=AOvVaw0709bky-w7TbDa1ql2Tz2v&amp;amp;opi=89978449" target="_blank"&gt;FlexCAN Bit Timing Calculation&lt;/A&gt;&amp;nbsp;document, and&amp;nbsp;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5xxx-S32Kxx-LPCxxxx-CAN-CAN-FD-bit-timing-calculation/ta-p/1119319" target="_blank"&gt;MPC5xxx/S32Kxx/LPCxxxx: CAN / CAN FD bit timing calculation&lt;/A&gt;&amp;nbsp;tool for clock and timing calculations.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Hope this is clear.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Aug 2026 18:14:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NXP-S32K312-CAN0-FIRC-vs-FXOSC-Clock-Source-Causing-CAN-Errors/m-p/2404657#M60468</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2026-08-13T18:14:29Z</dc:date>
    </item>
  </channel>
</rss>