<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Scrubbing ECC RAM in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Scrubbing-ECC-RAM/m-p/2403570#M60390</link>
    <description>&lt;P&gt;S32K1 devices do not support a hardware SRAM scrubbing mechanism that would automatically write corrected data back to memory after a correctable ECC event. A software-based implementation is also not feasible, as single-bit SRAM ECC correction events are not reported by the ERM, so the application cannot identify the affected memory location.&lt;/P&gt;
&lt;P&gt;While the S32K3 family also does not provide automatic SRAM scrubbing, it does report single-bit ECC events, which gives the application visibility into these errors and enables implementation of more advanced fault-handling strategies.&lt;/P&gt;</description>
    <pubDate>Tue, 11 Aug 2026 07:05:18 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2026-08-11T07:05:18Z</dc:date>
    <item>
      <title>Scrubbing ECC RAM</title>
      <link>https://community.nxp.com/t5/S32K/Scrubbing-ECC-RAM/m-p/2403508#M60379</link>
      <description>&lt;P&gt;MCU: S32K148&lt;/P&gt;&lt;P&gt;Driver: RTD 3.0.0&lt;/P&gt;&lt;P&gt;OS: Bare metal&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With the above MCU, is there a way of 'scrubbing' the ECC SRAM? 'Scrubbing' means that if a correctable error is detected, the SRAM cell is updated with the correct value if the user configures some appropriate registers. Some competing products such as TI Hercules have this feature.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Aug 2026 02:27:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Scrubbing-ECC-RAM/m-p/2403508#M60379</guid>
      <dc:creator>durga_choudhury</dc:creator>
      <dc:date>2026-08-11T02:27:34Z</dc:date>
    </item>
    <item>
      <title>Re: Scrubbing ECC RAM</title>
      <link>https://community.nxp.com/t5/S32K/Scrubbing-ECC-RAM/m-p/2403570#M60390</link>
      <description>&lt;P&gt;S32K1 devices do not support a hardware SRAM scrubbing mechanism that would automatically write corrected data back to memory after a correctable ECC event. A software-based implementation is also not feasible, as single-bit SRAM ECC correction events are not reported by the ERM, so the application cannot identify the affected memory location.&lt;/P&gt;
&lt;P&gt;While the S32K3 family also does not provide automatic SRAM scrubbing, it does report single-bit ECC events, which gives the application visibility into these errors and enables implementation of more advanced fault-handling strategies.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Aug 2026 07:05:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Scrubbing-ECC-RAM/m-p/2403570#M60390</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2026-08-11T07:05:18Z</dc:date>
    </item>
    <item>
      <title>Re: Scrubbing ECC RAM</title>
      <link>https://community.nxp.com/t5/S32K/Scrubbing-ECC-RAM/m-p/2403700#M60401</link>
      <description>Thank you very much for the feedback.</description>
      <pubDate>Tue, 11 Aug 2026 13:40:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Scrubbing-ECC-RAM/m-p/2403700#M60401</guid>
      <dc:creator>durga_choudhury</dc:creator>
      <dc:date>2026-08-11T13:40:59Z</dc:date>
    </item>
  </channel>
</rss>