<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Subject: Standalone Evaluation Software / GUI for MC33774A AFE (RD33774CNC3EVB)</title>
    <link>https://community.nxp.com/t5/S32K/Subject-Standalone-Evaluation-Software-GUI-for-MC33774A-AFE/m-p/2403151#M60335</link>
    <description>&lt;P&gt;Can we use&amp;nbsp;RD33774CNT3EVB(which is TPL based) for standalone testing as the mentioned part number is not available with us but&amp;nbsp;RD3374CNT3EVB id available along with the required setup&amp;nbsp;&lt;BR /&gt;&lt;LI-PRODUCT title="RD33774CNT3EVB" id="RD33774CNT3EVB"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 10 Aug 2026 04:39:50 GMT</pubDate>
    <dc:creator>sanket_dudhmande</dc:creator>
    <dc:date>2026-08-10T04:39:50Z</dc:date>
    <item>
      <title>Subject: Standalone Evaluation Software / GUI for MC33774A AFE (RD33774CNC3EVB)</title>
      <link>https://community.nxp.com/t5/S32K/Subject-Standalone-Evaluation-Software-GUI-for-MC33774A-AFE/m-p/2399839#M60103</link>
      <description>&lt;P&gt;I am working with the RD33774CNC3EVB (MC33774A-based CMU) and the RD-K358BMU evaluation board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like to evaluate and validate the MC33774A AFE independently, without integrating the complete BMS system. My goal is to verify features such as:&lt;/P&gt;&lt;P&gt;- Cell voltage measurements&lt;/P&gt;&lt;P&gt;- Temperature measurements&lt;/P&gt;&lt;P&gt;- Diagnostics and fault reporting&lt;/P&gt;&lt;P&gt;- Passive cell balancing&lt;/P&gt;&lt;P&gt;- Register configuration&lt;/P&gt;&lt;P&gt;- Communication between the BMU and AFE&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the following questions:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Does NXP provide a standalone evaluation GUI or PC software for the MC33774A?&lt;/P&gt;&lt;P&gt;2. Is there a FreeMASTER project, demonstration GUI, or any other graphical tool that can be used to monitor and configure the MC33774A through the BMU?&lt;/P&gt;&lt;P&gt;3. Is there a reference application or example firmware that enables evaluation of the MC33774A with minimal software development?&lt;/P&gt;&lt;P&gt;4. Are there any applications describing the recommended setup for evaluating the MC33774A using only the BMU and CMU evaluation boards?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My objective is to perform functional validation of the AFE before integrating it into a complete BMS system.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;BR /&gt;&lt;BR /&gt;&lt;LI-PRODUCT title="RD33774CNC3EVB" id="RD33774CNC3EVB"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;, &lt;LI-PRODUCT title="MC33774" id="MC33774"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;, &lt;LI-PRODUCT title="MC33665A" id="MC33665A"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Jul 2026 07:27:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Subject-Standalone-Evaluation-Software-GUI-for-MC33774A-AFE/m-p/2399839#M60103</guid>
      <dc:creator>sanket_dudhmande</dc:creator>
      <dc:date>2026-07-29T07:27:44Z</dc:date>
    </item>
    <item>
      <title>Re: Subject: Standalone Evaluation Software / GUI for MC33774A AFE (RD33774CNC3EVB)</title>
      <link>https://community.nxp.com/t5/S32K/Subject-Standalone-Evaluation-Software-GUI-for-MC33774A-AFE/m-p/2400420#M60132</link>
      <description>&lt;P&gt;Dear Sanket,&lt;/P&gt;
&lt;P&gt;1. Does NXP provide a standalone evaluation GUI or PC software for the MC33774A?&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;[A] Yes, there is an EvalGUI 7 for the&amp;nbsp;MC33774A. Specifically to be used with&amp;nbsp;RD33774ADSTEVB. The GUI is intended to be used with SPI interface for communication between MCU and SPI to TPL transceiver and then via TPL to the MC33774A. Please refer to the &lt;A href="https://www.nxp.com/docs/en/user-manual/UM11816.pdf" target="_self"&gt;UM11816&lt;/A&gt;.&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1785399710998.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393423i81F91CE18071C7F0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1785399710998.png" alt="JozefKozon_0-1785399710998.png" /&gt;&lt;/span&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;If you are asking if there is a GUI specifically for the&amp;nbsp;RD33774CNC3EVB with populated MC33665A TPL to CAN transceiver for the communication with MCU via CAN interface, unfortunately, there isn't any.&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;2. Is there a FreeMASTER project, demonstration GUI, or any other graphical tool that can be used to monitor and configure the MC33774A through the BMU?&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;[A] For the BMU and CMU boards you mentioned we have a whole software bundle. However you need an &lt;A href="https://www.nxp.com/design/design-center/software/automotive-software-and-tools/s32-design-studio-ide/s32-design-studio-for-s32-platform:S32DS-S32PLATFORM" target="_self"&gt;S32DS IDE&lt;/A&gt;. &lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_6-1785400949053.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393438i97CB80C99AACB8C6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_6-1785400949053.png" alt="JozefKozon_6-1785400949053.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;Please refer to this &lt;A href="https://www.nxp.com/app-autopackagemgr/automotive-software-package-manager:AUTO-SW-PACKAGE-MANAGER?currentTab=0&amp;amp;selectedDevices=S32K358" target="_self"&gt;link&lt;/A&gt;. Included are Demo projects for the FreeMASTER.&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_1-1785400007530.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393424iF4CFD2C7F8334098/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_1-1785400007530.png" alt="JozefKozon_1-1785400007530.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please refer to the Release Notes document on the right side.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_2-1785400038979.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393425i15719078DB2D8320/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_2-1785400038979.png" alt="JozefKozon_2-1785400038979.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;3. Is there a reference application or example firmware that enables evaluation of the MC33774A with minimal software development?&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;[A] See above what software is available for the EVBs you have. However, the two boards are not sufficient. You need your own battery pack, with minimally 4 Cells for each MC33774A, or we have&amp;nbsp;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/BATT-18EMULATOR?fpsp=1#documentation" target="_self"&gt;BATT-18EMULATOR&lt;/A&gt;. Emulating 18 Cells for each MC33774A populated on the&amp;nbsp;RD33774CNC3EVB.&amp;nbsp;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;SPAN&gt;Please refer to the &lt;A href="https://www.nxp.com/docs/en/user-manual/UM11943.pdf" target="_self"&gt;UM11943&lt;/A&gt;.&amp;nbsp;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_3-1785400370798.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393426iBB06E48FA429581F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_3-1785400370798.png" alt="JozefKozon_3-1785400370798.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_4-1785400486233.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393427i85549B3F8D6BF6AC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_4-1785400486233.png" alt="JozefKozon_4-1785400486233.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;4. Are there any applications describing the recommended setup for evaluating the MC33774A using only the BMU and CMU evaluation boards?&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;[A] Yes there is. However as mentioned above you need either a battery pack or the battery emulator. Please refer to the &lt;A href="https://www.nxp.com/docs/en/user-manual/UM11943.pdf" target="_self"&gt;UM11943&lt;/A&gt; and to this &lt;A href="https://www.nxp.com/document/guide/getting-started-with-the-rd33774cnc3evb-reference-design:GS-RD33774CNC3EVB" target="_self"&gt;link&lt;/A&gt;.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_5-1785400737734.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393435i0431B655999A8E51/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_5-1785400737734.png" alt="JozefKozon_5-1785400737734.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jul 2026 08:50:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Subject-Standalone-Evaluation-Software-GUI-for-MC33774A-AFE/m-p/2400420#M60132</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2026-07-30T08:50:29Z</dc:date>
    </item>
    <item>
      <title>Re: Subject: Standalone Evaluation Software / GUI for MC33774A AFE (RD33774CNC3EVB)</title>
      <link>https://community.nxp.com/t5/S32K/Subject-Standalone-Evaluation-Software-GUI-for-MC33774A-AFE/m-p/2403151#M60335</link>
      <description>&lt;P&gt;Can we use&amp;nbsp;RD33774CNT3EVB(which is TPL based) for standalone testing as the mentioned part number is not available with us but&amp;nbsp;RD3374CNT3EVB id available along with the required setup&amp;nbsp;&lt;BR /&gt;&lt;LI-PRODUCT title="RD33774CNT3EVB" id="RD33774CNT3EVB"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Aug 2026 04:39:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Subject-Standalone-Evaluation-Software-GUI-for-MC33774A-AFE/m-p/2403151#M60335</guid>
      <dc:creator>sanket_dudhmande</dc:creator>
      <dc:date>2026-08-10T04:39:50Z</dc:date>
    </item>
  </channel>
</rss>