<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: i.MX8M Mini driver USB HUB</title>
    <link>https://community.nxp.com/t5/S32K/i-MX8M-Mini-driver-USB-HUB/m-p/1006502#M6031</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you use the i.M8MM EVK board or the board you designed yourself? &lt;/P&gt;&lt;P&gt;If you are using the i.M8MM EVK board reference board, the default usb is type-c port, if you want to use the usb hub you need to use the special line.&lt;/P&gt;&lt;P&gt;If you want to design board yourself, you need to configure the usb to host mode and then connect the hub chip.&lt;/P&gt;&lt;P&gt;It depend on your hardware, the i.MX8MM support usb2.0, so drive needed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Nov 2019 07:33:48 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2019-11-15T07:33:48Z</dc:date>
    <item>
      <title>i.MX8M Mini driver USB HUB</title>
      <link>https://community.nxp.com/t5/S32K/i-MX8M-Mini-driver-USB-HUB/m-p/1006501#M6030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i.MX8M Mini can not drive USB HUB AX88772/AX88179 after i.MX8M Mini reset&amp;nbsp;without USB HUB, any update driver is OK now?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Nov 2019 07:37:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/i-MX8M-Mini-driver-USB-HUB/m-p/1006501#M6030</guid>
      <dc:creator>george_li</dc:creator>
      <dc:date>2019-11-05T07:37:26Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Mini driver USB HUB</title>
      <link>https://community.nxp.com/t5/S32K/i-MX8M-Mini-driver-USB-HUB/m-p/1006502#M6031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you use the i.M8MM EVK board or the board you designed yourself? &lt;/P&gt;&lt;P&gt;If you are using the i.M8MM EVK board reference board, the default usb is type-c port, if you want to use the usb hub you need to use the special line.&lt;/P&gt;&lt;P&gt;If you want to design board yourself, you need to configure the usb to host mode and then connect the hub chip.&lt;/P&gt;&lt;P&gt;It depend on your hardware, the i.MX8MM support usb2.0, so drive needed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Nov 2019 07:33:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/i-MX8M-Mini-driver-USB-HUB/m-p/1006502#M6031</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2019-11-15T07:33:48Z</dc:date>
    </item>
  </channel>
</rss>