<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Assistance Required for Flash Programming S32K344 Using USB Multilink Universal FX in S32 Design in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Assistance-Required-for-Flash-Programming-S32K344-Using-USB/m-p/2402623#M60279</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262505"&gt;@Aravind_Togaralli&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;1. NXP always recommends using the latest SW release available. Right now, the latest release for S32K3 include:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://nxp.flexnetoperations.com/control/frse/download?element=8103061" target="_blank"&gt;S32 Design Studio IDE 3.6.10&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://nxp.flexnetoperations.com/control/frse/download?element=7873971" target="_self"&gt; S32K3_S32M27x Real-Time Drivers ASR R23-11 Version 7.0.1&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;S32DS 3.6.10 includes PEmicro interface debugging support version 6.2.1.&lt;/P&gt;
&lt;P&gt;2. When importing an example, or creating a new S32DS application project, the respective debug configuration is generated. You can refer to the examples for the recommended settings, however, most important ones are 'C/C++ Application' path, device &amp;amp; port selected, and GDB Client executable path:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_1-1786048764074.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393902iE70214F2399D9366/image-size/large?v=v2&amp;amp;px=999" role="button" title="Julin_AragnM_1-1786048764074.png" alt="Julin_AragnM_1-1786048764074.png" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1786048752996.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393901i20704FC1FA6DA1DC/image-size/large?v=v2&amp;amp;px=999" role="button" title="Julin_AragnM_0-1786048752996.png" alt="Julin_AragnM_0-1786048752996.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;3. Yes, if you wish to debug the FRDM-A-S32K344 with an external debugger, you must use the&amp;nbsp;&lt;STRONG&gt;J9&lt;SPAN&gt;&amp;nbsp;20-pin Cortex Debug + ETM header.&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;4. As detailed inside the FRDM-A-S32K344 development board user manual (&lt;STRONG&gt;UM12406&lt;/STRONG&gt;), to enable this interface, jumper &lt;STRONG&gt;JP11 (OpenSDA voltage)&lt;/STRONG&gt; must be removed.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;5. You can refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Build-a-Project-and-Setup-Debugging-with-GDB-PEMicro/ta-p/1941848" target="_blank"&gt;HOWTO Build a Project and Setup Debugging with GDB PEMicro Debugging Interface&lt;/A&gt;. Or you can refer directly to PEmicro:&amp;nbsp;&lt;A href="https://www.pemicro.com/arm/device_support/NXP_Automotive/S32K3xx/index.cfm" target="_blank"&gt;PEmicro NXP_Automotive S32K3xx Device Support&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For any specific function/configuration, you can try contacting PEmicro instead.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 06 Aug 2026 20:46:15 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2026-08-06T20:46:15Z</dc:date>
    <item>
      <title>Assistance Required for Flash Programming S32K344 Using USB Multilink Universal FX in S32 Design Stu</title>
      <link>https://community.nxp.com/t5/S32K/Assistance-Required-for-Flash-Programming-S32K344-Using-USB/m-p/2402539#M60272</link>
      <description>&lt;P class=""&gt;Dear NXP Technical Support Team,&lt;/P&gt;&lt;P&gt;I hope you are doing well.&lt;/P&gt;&lt;P&gt;I am currently working with the &lt;STRONG&gt;FRDM-A-S32K344&lt;/STRONG&gt; evaluation board and using &lt;STRONG&gt;S32 Design Studio (S32DS)&lt;/STRONG&gt; for application development. I would like to program and debug the S32K344 MCU using a &lt;STRONG&gt;PEmicro USB Multilink Universal FX&lt;/STRONG&gt; debugger through the &lt;STRONG&gt;JTAG/SWD interface&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;I would appreciate your guidance on the correct configuration and setup for this hardware combination. Specifically, I would like assistance with the following:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;STRONG&gt;Software and Driver Requirements&lt;/STRONG&gt;&lt;UL&gt;&lt;LI&gt;Required PEmicro drivers and firmware versions.&lt;/LI&gt;&lt;LI&gt;Any additional S32DS packages or device support that must be installed.&lt;/LI&gt;&lt;LI&gt;Recommended version compatibility between S32DS and the USB Multilink Universal FX.&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;S32 Design Studio Debug Configuration&lt;/STRONG&gt;&lt;UL&gt;&lt;LI&gt;Step-by-step instructions for creating a &lt;STRONG&gt;PEmicro GDB Server&lt;/STRONG&gt; debug configuration.&lt;/LI&gt;&lt;LI&gt;Recommended settings for the &lt;STRONG&gt;Main&lt;/STRONG&gt;, &lt;STRONG&gt;Debugger&lt;/STRONG&gt;, &lt;STRONG&gt;Startup&lt;/STRONG&gt;, and &lt;STRONG&gt;Common&lt;/STRONG&gt; tabs.&lt;/LI&gt;&lt;LI&gt;Any target-specific configuration required for the S32K344.&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Hardware Connection&lt;/STRONG&gt;&lt;UL&gt;&lt;LI&gt;Confirmation of the correct JTAG/SWD pin connections between the &lt;STRONG&gt;FRDM-A-S32K344 J9 header&lt;/STRONG&gt; and the &lt;STRONG&gt;USB Multilink Universal FX (Port B)&lt;/STRONG&gt;.&lt;/LI&gt;&lt;LI&gt;Whether any special wiring or signal connections are recommended.&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Board Configuration&lt;/STRONG&gt;&lt;UL&gt;&lt;LI&gt;Required jumper or switch settings on the FRDM-A-S32K344 board.&lt;/LI&gt;&lt;LI&gt;Any configuration related to the &lt;STRONG&gt;FS26 System Basis Chip (SBC)&lt;/STRONG&gt; or watchdog that should be considered to prevent resets during programming and debugging.&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Reference Documentation&lt;/STRONG&gt;&lt;UL&gt;&lt;LI&gt;Any application notes, user guides, or example projects demonstrating the use of the &lt;STRONG&gt;USB Multilink Universal FX&lt;/STRONG&gt; with the &lt;STRONG&gt;S32K344&lt;/STRONG&gt; would be greatly appreciated.&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;For your reference, I have also attached a diagram illustrating the JTAG pin connections between the &lt;STRONG&gt;FRDM-A-S32K344 board&lt;/STRONG&gt; and the &lt;STRONG&gt;USB Multilink Universal FX&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Thank you for your time and support. I look forward to your guidance.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Aravind Togaralli&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Aug 2026 12:07:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Assistance-Required-for-Flash-Programming-S32K344-Using-USB/m-p/2402539#M60272</guid>
      <dc:creator>Aravind_Togaralli</dc:creator>
      <dc:date>2026-08-06T12:07:11Z</dc:date>
    </item>
    <item>
      <title>Re: Assistance Required for Flash Programming S32K344 Using USB Multilink Universal FX in S32 Design</title>
      <link>https://community.nxp.com/t5/S32K/Assistance-Required-for-Flash-Programming-S32K344-Using-USB/m-p/2402623#M60279</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262505"&gt;@Aravind_Togaralli&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;1. NXP always recommends using the latest SW release available. Right now, the latest release for S32K3 include:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://nxp.flexnetoperations.com/control/frse/download?element=8103061" target="_blank"&gt;S32 Design Studio IDE 3.6.10&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://nxp.flexnetoperations.com/control/frse/download?element=7873971" target="_self"&gt; S32K3_S32M27x Real-Time Drivers ASR R23-11 Version 7.0.1&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;S32DS 3.6.10 includes PEmicro interface debugging support version 6.2.1.&lt;/P&gt;
&lt;P&gt;2. When importing an example, or creating a new S32DS application project, the respective debug configuration is generated. You can refer to the examples for the recommended settings, however, most important ones are 'C/C++ Application' path, device &amp;amp; port selected, and GDB Client executable path:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_1-1786048764074.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393902iE70214F2399D9366/image-size/large?v=v2&amp;amp;px=999" role="button" title="Julin_AragnM_1-1786048764074.png" alt="Julin_AragnM_1-1786048764074.png" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1786048752996.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393901i20704FC1FA6DA1DC/image-size/large?v=v2&amp;amp;px=999" role="button" title="Julin_AragnM_0-1786048752996.png" alt="Julin_AragnM_0-1786048752996.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;3. Yes, if you wish to debug the FRDM-A-S32K344 with an external debugger, you must use the&amp;nbsp;&lt;STRONG&gt;J9&lt;SPAN&gt;&amp;nbsp;20-pin Cortex Debug + ETM header.&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;4. As detailed inside the FRDM-A-S32K344 development board user manual (&lt;STRONG&gt;UM12406&lt;/STRONG&gt;), to enable this interface, jumper &lt;STRONG&gt;JP11 (OpenSDA voltage)&lt;/STRONG&gt; must be removed.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;5. You can refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Build-a-Project-and-Setup-Debugging-with-GDB-PEMicro/ta-p/1941848" target="_blank"&gt;HOWTO Build a Project and Setup Debugging with GDB PEMicro Debugging Interface&lt;/A&gt;. Or you can refer directly to PEmicro:&amp;nbsp;&lt;A href="https://www.pemicro.com/arm/device_support/NXP_Automotive/S32K3xx/index.cfm" target="_blank"&gt;PEmicro NXP_Automotive S32K3xx Device Support&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For any specific function/configuration, you can try contacting PEmicro instead.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Aug 2026 20:46:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Assistance-Required-for-Flash-Programming-S32K344-Using-USB/m-p/2402623#M60279</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2026-08-06T20:46:15Z</dc:date>
    </item>
  </channel>
</rss>