<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K146 Package Selection without SDK</title>
    <link>https://community.nxp.com/t5/S32K/S32K146-Package-Selection-without-SDK/m-p/1005564#M6018</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using S32K146 144 Pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not using SDK for code generation &amp;amp; Configuring the Chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to change the package for S32K146. Kindly suggest a suitable way so as to select the package without using SDK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;BJ Rajendranath.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Feb 2020 13:32:33 GMT</pubDate>
    <dc:creator>bjrajendra</dc:creator>
    <dc:date>2020-02-10T13:32:33Z</dc:date>
    <item>
      <title>S32K146 Package Selection without SDK</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-Package-Selection-without-SDK/m-p/1005564#M6018</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using S32K146 144 Pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not using SDK for code generation &amp;amp; Configuring the Chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to change the package for S32K146. Kindly suggest a suitable way so as to select the package without using SDK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;BJ Rajendranath.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Feb 2020 13:32:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-Package-Selection-without-SDK/m-p/1005564#M6018</guid>
      <dc:creator>bjrajendra</dc:creator>
      <dc:date>2020-02-10T13:32:33Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 Package Selection without SDK</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-Package-Selection-without-SDK/m-p/1005565#M6019</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is the same header file for each package of S32K146.&lt;/P&gt;&lt;P&gt;So, you should just take care that you are using the pins available on your package.&lt;/P&gt;&lt;P&gt;The&amp;nbsp;pinout can be useful. It is available&amp;nbsp;in the RM&amp;nbsp;rev. 11. in the document&amp;nbsp;&lt;EM&gt;S32K146 IO_Signal_Description_Input_Multiplexing.xlsx&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2020 12:46:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-Package-Selection-without-SDK/m-p/1005565#M6019</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2020-02-11T12:46:41Z</dc:date>
    </item>
  </channel>
</rss>