<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RD33771CNTREVM + FreeMASTER project in S32K</title>
    <link>https://community.nxp.com/t5/S32K/RD33771CNTREVM-FreeMASTER-project/m-p/2400768#M60149</link>
    <description>&lt;P&gt;Hi Jozef,&lt;/P&gt;&lt;P&gt;Thank your the answer. I tried the&amp;nbsp;EvalGUI 5.15, but it lags on Windows 11 and it works only with COM port.&amp;nbsp;RD33771CNTREVM has CAN output...&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'll see if I can get the RX and TX signals out of the PCB. Then I could modify the original FW for the development kit to have the same input / output messages that EvalGUI 5.15 expects.&lt;/P&gt;&lt;P&gt;But I would still expect either PC SW or a FreeMASTER project for the development kit. That would be very helpful.&lt;/P&gt;</description>
    <pubDate>Fri, 31 Jul 2026 09:22:59 GMT</pubDate>
    <dc:creator>Marvin_Gjepali</dc:creator>
    <dc:date>2026-07-31T09:22:59Z</dc:date>
    <item>
      <title>RD33771CNTREVM + FreeMASTER project</title>
      <link>https://community.nxp.com/t5/S32K/RD33771CNTREVM-FreeMASTER-project/m-p/2400378#M60129</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am currently evaluating the RD33771CNTREVM (HV Battery Management System) reference design board.&lt;/P&gt;&lt;P&gt;According to the User Manual (UM11310), the board outputs raw register data via the CAN0 interface (connector J12). While I can read the raw hexadecimal messages using a standard CAN-USB interface, I am looking for a more efficient way to visualize the cell voltages and temperatures in real-time.&lt;/P&gt;&lt;P&gt;I noticed that for a similar silicon combination (S32K144 + MC33771C), NXP provides the BCC_S32K144_FreeMASTER example project within the BCC SW Driver Package.&lt;/P&gt;&lt;P&gt;Before I start modifying the pin routing and porting this generic example to match the specific hardware layout of the RD33771CNTREVM, I would like to ask:&lt;/P&gt;&lt;P&gt;Does NXP have a dedicated FreeMASTER project (.pmp / .pmpx) and the corresponding .elf firmware specifically tailored for the RD33771CNTREVM board?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for the support.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jul 2026 07:49:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RD33771CNTREVM-FreeMASTER-project/m-p/2400378#M60129</guid>
      <dc:creator>Marvin_Gjepali</dc:creator>
      <dc:date>2026-07-30T07:49:12Z</dc:date>
    </item>
    <item>
      <title>Re: RD33771CNTREVM + FreeMASTER project</title>
      <link>https://community.nxp.com/t5/S32K/RD33771CNTREVM-FreeMASTER-project/m-p/2400743#M60147</link>
      <description>&lt;P&gt;Hi Marvin,&lt;/P&gt;
&lt;P&gt;I have found an answer from an application team to another customer who requested FreeMASTER example for the&amp;nbsp;&lt;SPAN&gt;RD33771CNTREVM. Unfortunately we do not have any. We have only the EvalGUI. See the answer below. You can download the EvalGUI from the &lt;A href="https://www.nxp.com/products/MC33771C#documentation" target="_self"&gt;MC33771C product page&lt;/A&gt;. It is publicly available.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1785486988566.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393499i444DA5D3A69230E3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1785486988566.png" alt="JozefKozon_0-1785486988566.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;I apologize for inconvenience.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;DESCRIPTION&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;Unfortunately that is correct, the FreeMaster interface going with the example code has been developed for one node only. As is, it would not work with 4 nodes, only the first one would be initialized and monitored.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;For this distributed platform, the only GUI available for more than one node would be the EvalGUI 5.15..&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Fri, 31 Jul 2026 08:38:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RD33771CNTREVM-FreeMASTER-project/m-p/2400743#M60147</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2026-07-31T08:38:58Z</dc:date>
    </item>
    <item>
      <title>Re: RD33771CNTREVM + FreeMASTER project</title>
      <link>https://community.nxp.com/t5/S32K/RD33771CNTREVM-FreeMASTER-project/m-p/2400768#M60149</link>
      <description>&lt;P&gt;Hi Jozef,&lt;/P&gt;&lt;P&gt;Thank your the answer. I tried the&amp;nbsp;EvalGUI 5.15, but it lags on Windows 11 and it works only with COM port.&amp;nbsp;RD33771CNTREVM has CAN output...&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'll see if I can get the RX and TX signals out of the PCB. Then I could modify the original FW for the development kit to have the same input / output messages that EvalGUI 5.15 expects.&lt;/P&gt;&lt;P&gt;But I would still expect either PC SW or a FreeMASTER project for the development kit. That would be very helpful.&lt;/P&gt;</description>
      <pubDate>Fri, 31 Jul 2026 09:22:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RD33771CNTREVM-FreeMASTER-project/m-p/2400768#M60149</guid>
      <dc:creator>Marvin_Gjepali</dc:creator>
      <dc:date>2026-07-31T09:22:59Z</dc:date>
    </item>
    <item>
      <title>Re: RD33771CNTREVM + FreeMASTER project</title>
      <link>https://community.nxp.com/t5/S32K/RD33771CNTREVM-FreeMASTER-project/m-p/2400866#M60153</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi Marvin,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;currently there isn't any other software, apart from the software which you can find in the &lt;A href="https://www.nxp.com/products/MC33771C#documentation" target="_self"&gt;MC33771C&lt;/A&gt; and in the&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/flexible-battery-management-system-bms-reference-design:RD33771CNTREVM" target="_self"&gt;RD33771CNTREVM&lt;/A&gt; product pages. And since the MC33771C is an old product, although still in production, there probably will not be a new software. We have newer BCCs. For a new design I would rather recommend you one from the 24 or 26 Channels BCCs. BMA7x2x family. This are the latest BCC components.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/products/product-selector:PRODUCT-SELECTOR?category=c40_c328&amp;amp;page=1&amp;amp;nrnd=false" target="_blank"&gt;https://www.nxp.com/products/product-selector:PRODUCT-SELECTOR?category=c40_c328&amp;amp;page=1&amp;amp;nrnd=false&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1785495573469.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393519iBC6EE387495F8F41/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1785495573469.png" alt="JozefKozon_0-1785495573469.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Fri, 31 Jul 2026 11:00:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RD33771CNTREVM-FreeMASTER-project/m-p/2400866#M60153</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2026-07-31T11:00:05Z</dc:date>
    </item>
  </channel>
</rss>