<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Running Flex CAN with internal clock problem</title>
    <link>https://community.nxp.com/t5/S32K/Running-Flex-CAN-with-internal-clock-problem/m-p/1005228#M6004</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Swati Jha&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SIRC clock cannot be used as the FlexCAN oscillator clock.&amp;nbsp;FlexCAN oscillator clock is SOSCDIV2_CLK as mentioned in Table 27-9 of the reference manual.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Dec 2019 23:19:07 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2019-12-06T23:19:07Z</dc:date>
    <item>
      <title>Running Flex CAN with internal clock problem</title>
      <link>https://community.nxp.com/t5/S32K/Running-Flex-CAN-with-internal-clock-problem/m-p/1005227#M6003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone we are using s32k148 microcontroller we have running CAN application ,&lt;/P&gt;&lt;P&gt;please provide some reference code for FLEXCAN using SIRC clock source .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2019 07:05:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Running-Flex-CAN-with-internal-clock-problem/m-p/1005227#M6003</guid>
      <dc:creator>swati_jha</dc:creator>
      <dc:date>2019-12-04T07:05:06Z</dc:date>
    </item>
    <item>
      <title>Re: Running Flex CAN with internal clock problem</title>
      <link>https://community.nxp.com/t5/S32K/Running-Flex-CAN-with-internal-clock-problem/m-p/1005228#M6004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Swati Jha&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SIRC clock cannot be used as the FlexCAN oscillator clock.&amp;nbsp;FlexCAN oscillator clock is SOSCDIV2_CLK as mentioned in Table 27-9 of the reference manual.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Dec 2019 23:19:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Running-Flex-CAN-with-internal-clock-problem/m-p/1005228#M6004</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2019-12-06T23:19:07Z</dc:date>
    </item>
  </channel>
</rss>