<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックs32k324 write Dflash problem</title>
    <link>https://community.nxp.com/t5/S32K/s32k324-write-Dflash-problem/m-p/2396703#M59940</link>
    <description>&lt;P&gt;I used S32DS3.5 + RTD2.0 to develop S32K324. Now I wrote the program for the S32K324 based on the configuration and code in the example "Fee_Example_S32K344" and it compiled. but when it ran, the program would report an error as soon as it enters this code" Fls_Init(NULL_PTR);", when I step into it , I found it could not Skip this function " Fls_IPW_Init();". And the err made the program enter this function "&lt;BR /&gt;static inline void DevAssert(volatile boolean x)&lt;BR /&gt;{&lt;BR /&gt;if(x) { } else { for(;;) {ASM_KEYWORD(BREAKPOINT_INSTR);} }&lt;BR /&gt;}"&lt;BR /&gt;So I guess if the RTD version doesn't support S32K324 to use the fee function model ? Or could give me some other examples to write Dflash by eeprom mode of S32k324.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Mon, 20 Jul 2026 08:33:05 GMT</pubDate>
    <dc:creator>mmyjh_123</dc:creator>
    <dc:date>2026-07-20T08:33:05Z</dc:date>
    <item>
      <title>s32k324 write Dflash problem</title>
      <link>https://community.nxp.com/t5/S32K/s32k324-write-Dflash-problem/m-p/2396703#M59940</link>
      <description>&lt;P&gt;I used S32DS3.5 + RTD2.0 to develop S32K324. Now I wrote the program for the S32K324 based on the configuration and code in the example "Fee_Example_S32K344" and it compiled. but when it ran, the program would report an error as soon as it enters this code" Fls_Init(NULL_PTR);", when I step into it , I found it could not Skip this function " Fls_IPW_Init();". And the err made the program enter this function "&lt;BR /&gt;static inline void DevAssert(volatile boolean x)&lt;BR /&gt;{&lt;BR /&gt;if(x) { } else { for(;;) {ASM_KEYWORD(BREAKPOINT_INSTR);} }&lt;BR /&gt;}"&lt;BR /&gt;So I guess if the RTD version doesn't support S32K324 to use the fee function model ? Or could give me some other examples to write Dflash by eeprom mode of S32k324.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jul 2026 08:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k324-write-Dflash-problem/m-p/2396703#M59940</guid>
      <dc:creator>mmyjh_123</dc:creator>
      <dc:date>2026-07-20T08:33:05Z</dc:date>
    </item>
    <item>
      <title>Re: s32k324 write Dflash problem</title>
      <link>https://community.nxp.com/t5/S32K/s32k324-write-Dflash-problem/m-p/2396755#M59943</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/264835"&gt;@mmyjh_123&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Can you share the project or at least the .mex file?&lt;/P&gt;
&lt;P&gt;Also, you use a very old RTD.&lt;/P&gt;
&lt;P&gt;I would recommended upgrading to RTD 7.0.1.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jul 2026 11:19:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k324-write-Dflash-problem/m-p/2396755#M59943</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-07-20T11:19:05Z</dc:date>
    </item>
    <item>
      <title>Re: s32k324 write Dflash problem</title>
      <link>https://community.nxp.com/t5/S32K/s32k324-write-Dflash-problem/m-p/2396770#M59944</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Does the Fls_IPW_Init() generated by S32DS and is there any error log can be printed out?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jul 2026 11:35:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k324-write-Dflash-problem/m-p/2396770#M59944</guid>
      <dc:creator>db16122</dc:creator>
      <dc:date>2026-07-20T11:35:56Z</dc:date>
    </item>
    <item>
      <title>Re: s32k324 write Dflash problem</title>
      <link>https://community.nxp.com/t5/S32K/s32k324-write-Dflash-problem/m-p/2396956#M59955</link>
      <description>&lt;P&gt;Since all the project engineering was created based on RTD2.0, the migration might not be very convenient. It would be best if RTD2.0 could modify and use the Fee. Could you please help me review the program?&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jul 2026 01:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k324-write-Dflash-problem/m-p/2396956#M59955</guid>
      <dc:creator>mmyjh_123</dc:creator>
      <dc:date>2026-07-21T01:35:02Z</dc:date>
    </item>
    <item>
      <title>Re: s32k324 write Dflash problem</title>
      <link>https://community.nxp.com/t5/S32K/s32k324-write-Dflash-problem/m-p/2397332#M59971</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/264835"&gt;@mmyjh_123&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You have two options.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1.&lt;/P&gt;
&lt;P&gt;Either change it to&amp;nbsp;VARIANT-PRE-COMPILE&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1784639285437.png" style="width: 581px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/392802i3238DD7EC0DAC170/image-dimensions/581x167?v=v2" width="581" height="167" role="button" title="danielmartynek_0-1784639285437.png" alt="danielmartynek_0-1784639285437.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1784639285437.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;And call it as you do:&lt;/P&gt;
&lt;P&gt;Fls_Init(NULL_PTR);&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2.&lt;/P&gt;
&lt;P&gt;Or select&amp;nbsp;VARIANT-POST-BUILD instead&lt;/P&gt;
&lt;P&gt;and call:&lt;/P&gt;
&lt;P&gt;Fls_Init(&amp;amp;Fls_Config_BOARD_InitPeripherals);&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jul 2026 13:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k324-write-Dflash-problem/m-p/2397332#M59971</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-07-21T13:10:02Z</dc:date>
    </item>
    <item>
      <title>Re: s32k324 write Dflash problem</title>
      <link>https://community.nxp.com/t5/S32K/s32k324-write-Dflash-problem/m-p/2397470#M59979</link>
      <description>&lt;P&gt;Oh, I got it,thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jul 2026 02:08:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k324-write-Dflash-problem/m-p/2397470#M59979</guid>
      <dc:creator>mmyjh_123</dc:creator>
      <dc:date>2026-07-22T02:08:02Z</dc:date>
    </item>
  </channel>
</rss>