<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックUsing the MC34GD3000 Gate Driver with a 24 V BLDC Motor</title>
    <link>https://community.nxp.com/t5/S32K/Using-the-MC34GD3000-Gate-Driver-with-a-24-V-BLDC-Motor/m-p/2390852#M59704</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am currently using the S32K144 BLDC/PMSM Development Kit, which includes the MC34GD3000 gate driver IC.&lt;/P&gt;&lt;P&gt;From the application circuit and documentation, it appears that the reference design is intended for a 12 V BLDC motor. However, the BLDC motor included with the development kit is actually a 24 V motor, which raised a few questions for me.&lt;/P&gt;&lt;P&gt;I would appreciate your advice on the following:&lt;/P&gt;&lt;P&gt;My understanding is that the MC34GD3000 gate driver itself operates from a 12 V gate-drive supply, while the inverter DC bus can be supplied with 24 V for driving a 24 V BLDC motor. Is this the correct way to use the MC34GD3000, or am I missing something?&lt;BR /&gt;Are there any voltage-related limitations or precautions when using the MC34GD3000 with a 24 V BLDC motor? For example, are there any recommended operating conditions, bootstrap considerations, or other design points that I should pay attention to?&lt;BR /&gt;If anyone has experience using this development kit or the MC34GD3000 with a 24 V motor, I would greatly appreciate your advice.&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
    <pubDate>Mon, 06 Jul 2026 04:23:56 GMT</pubDate>
    <dc:creator>MCmuhyeon0523</dc:creator>
    <dc:date>2026-07-06T04:23:56Z</dc:date>
    <item>
      <title>Using the MC34GD3000 Gate Driver with a 24 V BLDC Motor</title>
      <link>https://community.nxp.com/t5/S32K/Using-the-MC34GD3000-Gate-Driver-with-a-24-V-BLDC-Motor/m-p/2390852#M59704</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am currently using the S32K144 BLDC/PMSM Development Kit, which includes the MC34GD3000 gate driver IC.&lt;/P&gt;&lt;P&gt;From the application circuit and documentation, it appears that the reference design is intended for a 12 V BLDC motor. However, the BLDC motor included with the development kit is actually a 24 V motor, which raised a few questions for me.&lt;/P&gt;&lt;P&gt;I would appreciate your advice on the following:&lt;/P&gt;&lt;P&gt;My understanding is that the MC34GD3000 gate driver itself operates from a 12 V gate-drive supply, while the inverter DC bus can be supplied with 24 V for driving a 24 V BLDC motor. Is this the correct way to use the MC34GD3000, or am I missing something?&lt;BR /&gt;Are there any voltage-related limitations or precautions when using the MC34GD3000 with a 24 V BLDC motor? For example, are there any recommended operating conditions, bootstrap considerations, or other design points that I should pay attention to?&lt;BR /&gt;If anyone has experience using this development kit or the MC34GD3000 with a 24 V motor, I would greatly appreciate your advice.&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
      <pubDate>Mon, 06 Jul 2026 04:23:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-the-MC34GD3000-Gate-Driver-with-a-24-V-BLDC-Motor/m-p/2390852#M59704</guid>
      <dc:creator>MCmuhyeon0523</dc:creator>
      <dc:date>2026-07-06T04:23:56Z</dc:date>
    </item>
    <item>
      <title>Re: Using the MC34GD3000 Gate Driver with a 24 V BLDC Motor</title>
      <link>https://community.nxp.com/t5/S32K/Using-the-MC34GD3000-Gate-Driver-with-a-24-V-BLDC-Motor/m-p/2390940#M59707</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;MCmuhyeon0523&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;you can take a look this solution,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The MCSXTE2BK142 is a development board engineered for 3-phase Permanent Magnet (BLDC/PMSM) motor up to 800 W output at 24 V system or up to 400 W at 12 V system.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/MCSXTE2BK142" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/MCSXTE2BK142&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Jul 2026 07:33:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-the-MC34GD3000-Gate-Driver-with-a-24-V-BLDC-Motor/m-p/2390940#M59707</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2026-07-06T07:33:12Z</dc:date>
    </item>
  </channel>
</rss>